<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB to OTG port on MCIMX6Q-SDB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-to-OTG-port-on-MCIMX6Q-SDB/m-p/427012#M64759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tracy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just tested “android_L5.0.0_1.0.0-ga_images_6qsabresd” demo images on SABRE_SD with a mouse/keyboard connected to the OTG USB port, and everything worked properly.&lt;/P&gt;&lt;P&gt;If you still having issues, could you please specify where is mentioned that keyboard/mouse are not supported?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Oct 2015 22:59:30 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2015-10-12T22:59:30Z</dc:date>
    <item>
      <title>USB to OTG port on MCIMX6Q-SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-to-OTG-port-on-MCIMX6Q-SDB/m-p/427011#M64758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why is the OTG/USB keyboard and mouse considered not supported on android_L5.0.0_1.0.0 and related kernel builds on the MCIMX6Q-SDB? The board has the OTG port.&amp;nbsp; Using a 6 inch micro B male to USB A female OTG cable to the OTG port and either connecting a 3.0 USB HUB or keyboard directly into the USB A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Similar bug was found and the suggested fix was to deselect USB_OTG_FSM.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this the correct solution and why on freescales L5.0.0_1.0.0-ga_core_image_6qsabresd pre-built image?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If OTG_FSM is deselected, will the USB-OTG cable function as a USB straight through cable without the USB 2.0 USB_OTG_FSM support?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;usb 1-1.1: new full speed USB device number 7 using fsl-ehci (3.0 USB hub used)&lt;/P&gt;&lt;P&gt;usb 1-1.1: device v046d pc52b is not supported&lt;/P&gt;&lt;P&gt;usb 1-1: device v04f2 p0112 is not supported&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;usb 1-1: new low speed USB device number 3 using fsl-ehci (keyboard directly attached to the USB-OTG cable)&lt;/P&gt;&lt;P&gt;usb 1-1: device v413c p2107 is not supported &lt;/P&gt;&lt;P&gt;input: DELL Dell USB Entry Keyboard as /devices/platform/fsl-ehci.0/usb1/1-1/1-10&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Oct 2015 22:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-to-OTG-port-on-MCIMX6Q-SDB/m-p/427011#M64758</guid>
      <dc:creator>Gandalf-kern</dc:creator>
      <dc:date>2015-10-01T22:28:24Z</dc:date>
    </item>
    <item>
      <title>Re: USB to OTG port on MCIMX6Q-SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-to-OTG-port-on-MCIMX6Q-SDB/m-p/427012#M64759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tracy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just tested “android_L5.0.0_1.0.0-ga_images_6qsabresd” demo images on SABRE_SD with a mouse/keyboard connected to the OTG USB port, and everything worked properly.&lt;/P&gt;&lt;P&gt;If you still having issues, could you please specify where is mentioned that keyboard/mouse are not supported?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Oct 2015 22:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-to-OTG-port-on-MCIMX6Q-SDB/m-p/427012#M64759</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-10-12T22:59:30Z</dc:date>
    </item>
    <item>
      <title>Re: USB to OTG port on MCIMX6Q-SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-to-OTG-port-on-MCIMX6Q-SDB/m-p/427013#M64760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos, The serial console keyboard and a keyboard attached to the OTG/USB port issue was because of forgetting to set both hardware and software flow control to No in sudo minicom -s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Serial /dev/ttyUSB0&lt;/P&gt;&lt;P&gt;115200 8N1&lt;/P&gt;&lt;P&gt;HD flow no&lt;/P&gt;&lt;P&gt;SF flow no&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The HDMI display works with a HDMI cable from the HDMI port to the HDMI display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for taking time to look at this. They keyboard is supported.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Oct 2015 23:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-to-OTG-port-on-MCIMX6Q-SDB/m-p/427013#M64760</guid>
      <dc:creator>Gandalf-kern</dc:creator>
      <dc:date>2015-10-12T23:31:01Z</dc:date>
    </item>
  </channel>
</rss>