<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAndroid build for MCIMX6Q-SDB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-build-for-MCIMX6Q-SDB/m-p/426980#M64745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which of these two builds work correctly on the MCIMX6Q-SDB, or which is the correct BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sabreauto_6q i.MX 6Quad Auto Infotainment&lt;/P&gt;&lt;P&gt;sabresd_6dq i.MX 6DualQuad SABRE Board and SABRE Platform&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are taken from the android_L5.0.0_1.0.0-ga_... published/Android User's Guide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Oct 2015 22:13:08 GMT</pubDate>
    <dc:creator>Gandalf-kern</dc:creator>
    <dc:date>2015-10-01T22:13:08Z</dc:date>
    <item>
      <title>Android build for MCIMX6Q-SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-build-for-MCIMX6Q-SDB/m-p/426980#M64745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which of these two builds work correctly on the MCIMX6Q-SDB, or which is the correct BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sabreauto_6q i.MX 6Quad Auto Infotainment&lt;/P&gt;&lt;P&gt;sabresd_6dq i.MX 6DualQuad SABRE Board and SABRE Platform&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are taken from the android_L5.0.0_1.0.0-ga_... published/Android User's Guide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Oct 2015 22:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-build-for-MCIMX6Q-SDB/m-p/426980#M64745</guid>
      <dc:creator>Gandalf-kern</dc:creator>
      <dc:date>2015-10-01T22:13:08Z</dc:date>
    </item>
    <item>
      <title>Re: Android build for MCIMX6Q-SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-build-for-MCIMX6Q-SDB/m-p/426981#M64746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCIMX6Q-SDB relates to sabresd_6dq i.MX 6DualQuad SABRE Board and SABRE Platform.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2015 01:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-build-for-MCIMX6Q-SDB/m-p/426981#M64746</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-02T01:41:23Z</dc:date>
    </item>
  </channel>
</rss>