<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Modification of DDR Stress Test for i.MX53 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Modification-of-DDR-Stress-Test-for-i-MX53/m-p/426564#M64654</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to run DDR Stress Tester on the cutomer original iMX53 board.&lt;BR /&gt;However, I need to change to UART-4 port from UART-1 port.&lt;BR /&gt;The UART4 port is below.&lt;/P&gt;&lt;P&gt;-TXD CSI0_DATA12/ALT2&lt;BR /&gt;-RXD CSI0_DATA13/ALT3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which part of source code do I change ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;*I have already got a source code of the DDR_Stress_Tester_for_mx51mx53_V002 from FSL local FAE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ko-hey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jul 2015 06:32:13 GMT</pubDate>
    <dc:creator>ko-hey</dc:creator>
    <dc:date>2015-07-21T06:32:13Z</dc:date>
    <item>
      <title>Modification of DDR Stress Test for i.MX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Modification-of-DDR-Stress-Test-for-i-MX53/m-p/426564#M64654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to run DDR Stress Tester on the cutomer original iMX53 board.&lt;BR /&gt;However, I need to change to UART-4 port from UART-1 port.&lt;BR /&gt;The UART4 port is below.&lt;/P&gt;&lt;P&gt;-TXD CSI0_DATA12/ALT2&lt;BR /&gt;-RXD CSI0_DATA13/ALT3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which part of source code do I change ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;*I have already got a source code of the DDR_Stress_Tester_for_mx51mx53_V002 from FSL local FAE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ko-hey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 06:32:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Modification-of-DDR-Stress-Test-for-i-MX53/m-p/426564#M64654</guid>
      <dc:creator>ko-hey</dc:creator>
      <dc:date>2015-07-21T06:32:13Z</dc:date>
    </item>
    <item>
      <title>Re: Modification of DDR Stress Test for i.MX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Modification-of-DDR-Stress-Test-for-i-MX53/m-p/426565#M64655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ko-hey&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can add codes to function debug_uart_iomux() in hardware.c&lt;/P&gt;&lt;P&gt;alternatively one can add uart4 iomux settings in *.inc file like&lt;/P&gt;&lt;P&gt;..\DDR_Stress_Tester_for_mx51mx53_V002\binary\MX53_TO2_DDR3_LCB.inc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 11:54:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Modification-of-DDR-Stress-Test-for-i-MX53/m-p/426565#M64655</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-21T11:54:13Z</dc:date>
    </item>
  </channel>
</rss>