<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: PF0100 SW1 current for i.MX6 Quad</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1-current-for-i-MX6-Quad/m-p/426442#M64633</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the idea&amp;nbsp;that the PMIC is able to handle some momentary high current spikes, however if the layout has not been given enough width or any poor soldering along the path where the current is needed, what will the processor experience when voltage drops (for a short moment) in those VDD_ARM and VDD_SOC pins? Is it a disgraceful black out or a temporary freeze which will come back immediately right after the current stabilized?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kok Suan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 May 2017 06:03:17 GMT</pubDate>
    <dc:creator>koksuanliew</dc:creator>
    <dc:date>2017-05-29T06:03:17Z</dc:date>
    <item>
      <title>PF0100 SW1 current for i.MX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1-current-for-i-MX6-Quad/m-p/426440#M64631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We design a board using i.MX6Quad and PF0100.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We look at datasheets of i.MX6Qual and PF0100.&lt;BR /&gt;However, we think that Currents of SW1A/B and SW1C of PF0100 are not enough.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How should we understand this in designing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the SBRE-SD board, these are connected as follows.&lt;/P&gt;&lt;P&gt;- PF0100 SW1A/B [2500mA] =&amp;gt; i.MX6Q VDDCORE(VDD_ARM_IN+VDD_ARM23_IN) [Max 3730mA]&lt;BR /&gt;- PF0100 SW1C [2000mA] =&amp;gt; i.MX6Q VDDSOC(VDD_SOC_IN) [Max 2370mA]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For i.MX6Quad&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="imx6 max supply.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3010i0BA3124C1FB47CDA/image-size/large?v=v2&amp;amp;px=999" role="button" title="imx6 max supply.png" alt="imx6 max supply.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For PF0100&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="PF0100 Power Tree.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26328i116EDE0C3FA552B2/image-size/large?v=v2&amp;amp;px=999" role="button" title="PF0100 Power Tree.png" alt="PF0100 Power Tree.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May I have advice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2015 11:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1-current-for-i-MX6-Quad/m-p/426440#M64631</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2015-11-19T11:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 SW1 current for i.MX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1-current-for-i-MX6-Quad/m-p/426441#M64632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The values of 3730mA for VDD_ARM_IN + VDD_ARM23_IN and 2370mA for VDD_SOC_IN are absolutely worst case values that are not typically achieved in real life operation. Also, as per the Table 54, sections "SW1A/B (SINGLE/DUAL PHASE)" and "SW1C (INDEPENDENT)", these regulators can provide the currents higher than 2.5A/2A for a short period of time.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Nov 2015 13:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1-current-for-i-MX6-Quad/m-p/426441#M64632</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-11-23T13:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 SW1 current for i.MX6 Quad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1-current-for-i-MX6-Quad/m-p/426442#M64633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the idea&amp;nbsp;that the PMIC is able to handle some momentary high current spikes, however if the layout has not been given enough width or any poor soldering along the path where the current is needed, what will the processor experience when voltage drops (for a short moment) in those VDD_ARM and VDD_SOC pins? Is it a disgraceful black out or a temporary freeze which will come back immediately right after the current stabilized?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kok Suan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 May 2017 06:03:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1-current-for-i-MX6-Quad/m-p/426442#M64633</guid>
      <dc:creator>koksuanliew</dc:creator>
      <dc:date>2017-05-29T06:03:17Z</dc:date>
    </item>
  </channel>
</rss>