<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 RTC_XTAL bumps</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426438#M64629</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, if an external RTC oscillator is not use, the i.MX6 will switches to the internal ring oscillator, but when I didn't use an external RTC, few boards sometime will not boot and reboot, it just stop and cannot see message from UART debug port. I assert POR signal, iMX6 still not work.&lt;/P&gt;&lt;P&gt;But when I connect RTC_XTALI with 4.7k to ground, the symptom was never happen again. Is it any problem with software or hardware setting?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jun 2015 03:00:25 GMT</pubDate>
    <dc:creator>chenjasper</dc:creator>
    <dc:date>2015-06-25T03:00:25Z</dc:date>
    <item>
      <title>i.MX6 RTC_XTAL bumps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426436#M64627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In IMX6DQRM Revision 2, 71.1 it said Automatically switch to the external oscillation source when sensed on the RTC_XTAL bumps(contacts) (32 kHz specific feature). Is it means i.MX6 sensed it by checking XTALOSC_RTC_XTALI &amp;amp; XTALOSC_RTC_XTALO pin contact with external oscillator or not?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 14:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426436#M64627</guid>
      <dc:creator>m_c</dc:creator>
      <dc:date>2015-06-24T14:44:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 RTC_XTAL bumps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426437#M64628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are correct. In case the i.MX6 detects that an external oscillator has been connected to the XTALOSC_RTC_XTALI &amp;amp; XTALOSC_RTC_XTALO pins this external oscillator is used. In the absence of an external RTC oscillator the i.MX6 switches to the internal ring oscillator. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;More details on this on-chip oscillator can be found on Section 4.1.4 of the i.MX6DQ Datasheet. I recommend reviewing these as the on-chip oscillator is not as precise as a 32 kHz crystal.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 16:40:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426437#M64628</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-06-24T16:40:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 RTC_XTAL bumps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426438#M64629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, if an external RTC oscillator is not use, the i.MX6 will switches to the internal ring oscillator, but when I didn't use an external RTC, few boards sometime will not boot and reboot, it just stop and cannot see message from UART debug port. I assert POR signal, iMX6 still not work.&lt;/P&gt;&lt;P&gt;But when I connect RTC_XTALI with 4.7k to ground, the symptom was never happen again. Is it any problem with software or hardware setting?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2015 03:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426438#M64629</guid>
      <dc:creator>chenjasper</dc:creator>
      <dc:date>2015-06-25T03:00:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 RTC_XTAL bumps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426439#M64630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chen Jasper,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is normal HW behavior. In order to engage the internal on-chip loose-tolerance ring oscillator you need to tie RTC_XTALI to GND and leave RTC_XTALO floated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 17:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-RTC-XTAL-bumps/m-p/426439#M64630</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-07-08T17:44:00Z</dc:date>
    </item>
  </channel>
</rss>