<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Mfgtool source for 3.10.17 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426243#M64580</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Building imx_v7_mfg_defconfig will give us uImage with Mfgtool support. That's fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But for our board each time we flash and reboot, the u-boot is &lt;STRONG&gt;default 1GB&lt;/STRONG&gt; ram which is same as the Mfgtool's u-boot. But if you see the Mfgtool directory structure, "files" directory contains the images to be flashed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's exactly not happening for "u-boot" only. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uImage and filesystem are flashed okay but not u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My guess was that, once the DDR is initialized with 1GB ram, even though i tried flashing 2GB configuration u-boot, the MFGtool is not able to flash that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's why i wanted to try this method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What i want is, the source for u-boot with which the MfgTool u-boot is configured with.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jul 2015 09:20:41 GMT</pubDate>
    <dc:creator>manjunathjoshi</dc:creator>
    <dc:date>2015-07-21T09:20:41Z</dc:date>
    <item>
      <title>Mfgtool source for 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426241#M64578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can anyone tell me where is the source for Mfgtool 3.10.17 for u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In ucl2 file,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we have,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;&amp;lt;CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/&lt;STRONG&gt;u-boot-imx6q%board%_sd.imx&lt;/STRONG&gt;" ifdev="MX6Q"&amp;gt;Loading U-boot&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This u-boot considers default 1GB ram but our board has 2gb ram. So i want to modify source code and use the MfgTool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 04:53:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426241#M64578</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2015-07-21T04:53:49Z</dc:date>
    </item>
    <item>
      <title>Re: Mfgtool source for 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426242#M64579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manjunath&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at attched Yocto User Guide sect.6.3 MFGTool.&lt;/P&gt;&lt;P&gt;The manufacturing defconfig is imx_v7_mfg_defconfig and this is required&lt;/P&gt;&lt;P&gt;for the fsl-image-manufacturing image for the manufacturing tools support.&lt;/P&gt;&lt;P&gt;Yocto building is described on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1616"&gt;Freescale Yocto Project main page&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 06:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426242#M64579</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-21T06:26:04Z</dc:date>
    </item>
    <item>
      <title>Re: Mfgtool source for 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426243#M64580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Building imx_v7_mfg_defconfig will give us uImage with Mfgtool support. That's fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But for our board each time we flash and reboot, the u-boot is &lt;STRONG&gt;default 1GB&lt;/STRONG&gt; ram which is same as the Mfgtool's u-boot. But if you see the Mfgtool directory structure, "files" directory contains the images to be flashed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's exactly not happening for "u-boot" only. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uImage and filesystem are flashed okay but not u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My guess was that, once the DDR is initialized with 1GB ram, even though i tried flashing 2GB configuration u-boot, the MFGtool is not able to flash that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's why i wanted to try this method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What i want is, the source for u-boot with which the MfgTool u-boot is configured with.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 09:20:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426243#M64580</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2015-07-21T09:20:41Z</dc:date>
    </item>
    <item>
      <title>Re: Mfgtool source for 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426244#M64581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manjunath&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uboot can be built separately please refer to attached Porting Guide&lt;/P&gt;&lt;P&gt;Chapter 1 Porting U-Boot. DDR configuration is defined in&lt;/P&gt;&lt;P&gt;..include/configs/mx6qsabresd.h,mx6qsabresd_mfg.h,mx6_common.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 12:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-source-for-3-10-17/m-p/426244#M64581</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-21T12:29:48Z</dc:date>
    </item>
  </channel>
</rss>