<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: DDR Stress Test v1.0.3 vs. v2.20</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425805#M64518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as it's been a while I posted this, I can hardly remember, what exactly I did.&lt;/P&gt;&lt;P&gt;The current version of Stress Test Tool allows entering the MR1 value manually, so there is no need to get it from the init file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached the file, that worked for me...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Feb 2017 09:58:56 GMT</pubDate>
    <dc:creator>mahi</dc:creator>
    <dc:date>2017-02-08T09:58:56Z</dc:date>
    <item>
      <title>DDR Stress Test v1.0.3 vs. v2.20</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425801#M64514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;there are some threads about this topic but I could not find a solution yet.&lt;/P&gt;&lt;P&gt;My DDR3 init script seems to work with the "old" DDR Stress Test tool. But when trying to use the current tool, "DQS gating calibration" fails. It seem to be due to the MR1 value which is not read from the init file correctly.&lt;/P&gt;&lt;P&gt;According to &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-105652#comment-31888"&gt;https://community.freescale.com/docs/DOC-105652#comment-31888&lt;/A&gt; changing the last line &lt;SPAN style="font-family: courier new,courier;"&gt;setmem /32 0x021b001c = 0x00000000&lt;/SPAN&gt; of the Script-Aid generated script to &lt;SPAN style="font-family: courier new,courier;"&gt;setmem /32 0x021b001c = 0x00040000&lt;/SPAN&gt; should tell the new Stress Test tool to use a MR1 value of 4. But when looking at the output of the tool, it keeps saying "ddr_mr1=0x00000000".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt; Martin&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336996"&gt;InitScript.inc.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Oct 2015 08:27:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425801#M64514</guid>
      <dc:creator>mahi</dc:creator>
      <dc:date>2015-10-26T08:27:52Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Stress Test v1.0.3 vs. v2.20</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425802#M64515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I think, it makes sense to post this issue&amp;nbsp; to &lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.20&lt;/A&gt; &lt;/P&gt;&lt;P&gt;directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Nov 2015 07:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425802#M64515</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-11-06T07:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Stress Test v1.0.3 vs. v2.20</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425803#M64516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The new version 2.30 (see &lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.30&lt;/A&gt;) finally fixes this issue - now it works perfectly...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Nov 2015 07:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425803#M64516</guid>
      <dc:creator>mahi</dc:creator>
      <dc:date>2015-11-23T07:52:55Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Stress Test v1.0.3 vs. v2.20</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425804#M64517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DDR Stress Test Tool V2.60 doesn't recognize my MR1 value.&lt;/P&gt;&lt;P&gt;Even if i use your attached init script with DDR Stress Test Tool V2.60 it doesn't set MR1 correctly (it stays at 0000).&lt;/P&gt;&lt;P&gt;Do you remember if you had to change something, maybe formatting, so it works?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Feb 2017 07:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425804#M64517</guid>
      <dc:creator>versat</dc:creator>
      <dc:date>2017-02-02T07:39:52Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Stress Test v1.0.3 vs. v2.20</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425805#M64518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as it's been a while I posted this, I can hardly remember, what exactly I did.&lt;/P&gt;&lt;P&gt;The current version of Stress Test Tool allows entering the MR1 value manually, so there is no need to get it from the init file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached the file, that worked for me...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2017 09:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Stress-Test-v1-0-3-vs-v2-20/m-p/425805#M64518</guid>
      <dc:creator>mahi</dc:creator>
      <dc:date>2017-02-08T09:58:56Z</dc:date>
    </item>
  </channel>
</rss>