<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Issues writing an SD card image from Ubuntu under VirtualBox in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issues-writing-an-SD-card-image-from-Ubuntu-under-VirtualBox/m-p/425668#M64486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to write an sdcard image created with a completely stock Yocto build (which completed successfully).&amp;nbsp; Following the instructions (including the sync at the end), I dd the .sdcard image onto the SD card.&amp;nbsp; Unfortunately, when I try to boot (the system does show signs of life and does start the boot process), I see all sorts of warnings on the serial console that point to a corrupt filesystem, and things end in a hang or a kernel panic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running Ubuntu 14.04LTS (I've tried 12.04 as well) under VirtualBox 4.3.20 running on a Windows 7 box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If anyone's had success with a similar config, any hints on what may be wrong?&amp;nbsp; Any recommendations for particular SD cards or SD card readers that you've had success with?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 09 Aug 2015 20:15:29 GMT</pubDate>
    <dc:creator>bricdesigns</dc:creator>
    <dc:date>2015-08-09T20:15:29Z</dc:date>
    <item>
      <title>Issues writing an SD card image from Ubuntu under VirtualBox</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-writing-an-SD-card-image-from-Ubuntu-under-VirtualBox/m-p/425668#M64486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to write an sdcard image created with a completely stock Yocto build (which completed successfully).&amp;nbsp; Following the instructions (including the sync at the end), I dd the .sdcard image onto the SD card.&amp;nbsp; Unfortunately, when I try to boot (the system does show signs of life and does start the boot process), I see all sorts of warnings on the serial console that point to a corrupt filesystem, and things end in a hang or a kernel panic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running Ubuntu 14.04LTS (I've tried 12.04 as well) under VirtualBox 4.3.20 running on a Windows 7 box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If anyone's had success with a similar config, any hints on what may be wrong?&amp;nbsp; Any recommendations for particular SD cards or SD card readers that you've had success with?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Aug 2015 20:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-writing-an-SD-card-image-from-Ubuntu-under-VirtualBox/m-p/425668#M64486</guid>
      <dc:creator>bricdesigns</dc:creator>
      <dc:date>2015-08-09T20:15:29Z</dc:date>
    </item>
    <item>
      <title>Re: Issues writing an SD card image from Ubuntu under VirtualBox</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-writing-an-SD-card-image-from-Ubuntu-under-VirtualBox/m-p/425669#M64487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to discard connection issues on SD card reader connection between host PC with virtualized system has issues, you should try generating the bootable SD card using the pre-compiled Yocto demo images. Please refer to the “DEMO_BSPs” downloadable from “Operating System Software-Board Support Packages” section of the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;SABRE for Smart Devices Reference Design|Freescale&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a recommendation for virtualized OS, is using a USB card reader, instead of using the integrated SD reader of some computers, as USB devices are better routable between host and virtualized systems.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 23:57:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-writing-an-SD-card-image-from-Ubuntu-under-VirtualBox/m-p/425669#M64487</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-08-10T23:57:54Z</dc:date>
    </item>
    <item>
      <title>Re: Issues writing an SD card image from Ubuntu under VirtualBox</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-writing-an-SD-card-image-from-Ubuntu-under-VirtualBox/m-p/425670#M64488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for a great suggestion.&amp;nbsp; That definitely would have been a faster path to test than my compiles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I actually got things to work finally after I changed two things.&amp;nbsp; First, instead of removing the SD card reader each time I wanted to swap the SD card around, I left the SD card reader connected to my PC and just removed and inserted the SD card.&amp;nbsp; This let the SD card reader stay assigned to the VM and made it so that Windows didn't keep getting involved.&amp;nbsp; The more likely fix was actually the second thing - when I was inserting the SD card reader each time, Ubuntu was automatically mounting the partitions that it found, and I wasn't unmounting them before I did the dd.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So after I inserted the SD card with the SD card reader already connected to my PC and assigned to my Ubuntu VM and after unmounting the existing partitions on the SD card, I was able to successfully dd the image and boot my iMX6 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 04:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-writing-an-SD-card-image-from-Ubuntu-under-VirtualBox/m-p/425670#M64488</guid>
      <dc:creator>bricdesigns</dc:creator>
      <dc:date>2015-08-11T04:37:44Z</dc:date>
    </item>
  </channel>
</rss>