<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMMPF0100 VGEN4 1.8V</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-VGEN4-1-8V/m-p/425647#M64482</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We had received Default Configuration of MMPF0100, The default voltage at VGEN4 is not got. All other regulator outputs are proper.&lt;/P&gt;&lt;P&gt;Kindly suggest what may be the issue. The&amp;nbsp; input to PMIC (VIN) is 3.4V. If suppose we power up the PMIC through Battery , the input Voltage will go upto 4.2 V. &lt;/P&gt;&lt;P&gt;Is there any proplem for the regulators, since VGEN4 Input regulator VIN max is 3.6 V???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Sylvia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jun 2015 07:35:30 GMT</pubDate>
    <dc:creator>sylvia</dc:creator>
    <dc:date>2015-06-04T07:35:30Z</dc:date>
    <item>
      <title>MMPF0100 VGEN4 1.8V</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-VGEN4-1-8V/m-p/425647#M64482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We had received Default Configuration of MMPF0100, The default voltage at VGEN4 is not got. All other regulator outputs are proper.&lt;/P&gt;&lt;P&gt;Kindly suggest what may be the issue. The&amp;nbsp; input to PMIC (VIN) is 3.4V. If suppose we power up the PMIC through Battery , the input Voltage will go upto 4.2 V. &lt;/P&gt;&lt;P&gt;Is there any proplem for the regulators, since VGEN4 Input regulator VIN max is 3.6 V???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Sylvia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 07:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-VGEN4-1-8V/m-p/425647#M64482</guid>
      <dc:creator>sylvia</dc:creator>
      <dc:date>2015-06-04T07:35:30Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC MMPF0100 VGEN4 1.8V Default Voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-VGEN4-1-8V/m-p/425648#M64483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please check Your design regarding the Startup erratum &lt;/P&gt;&lt;P&gt;(False start and/or non-start of regulators).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf?fasp=1" title="http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf?fasp=1"&gt;http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2015 06:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-VGEN4-1-8V/m-p/425648#M64483</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-06-05T06:24:11Z</dc:date>
    </item>
  </channel>
</rss>