<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 SD Card maximum PCB Track Lenghts  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD-Card-maximum-PCB-Track-Lenghts/m-p/425645#M64480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question about the maximum PCB signal track lengths for the SD interface : &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because of the tight PCB space and other mechanical limitations, the best we can place the Micro SD connector is 3.5 inches away from the i.MX6 DualLite. Which makes the SD track lengths around 4 inches long. We would like to run the SD interface at SDR12 speed (25MHz).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is 4 inches of track length acceptable for SD interface to work at 25MHz? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Selcuk&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Nov 2015 15:50:59 GMT</pubDate>
    <dc:creator>skuzu</dc:creator>
    <dc:date>2015-11-19T15:50:59Z</dc:date>
    <item>
      <title>i.MX6 SD Card maximum PCB Track Lenghts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD-Card-maximum-PCB-Track-Lenghts/m-p/425645#M64480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question about the maximum PCB signal track lengths for the SD interface : &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because of the tight PCB space and other mechanical limitations, the best we can place the Micro SD connector is 3.5 inches away from the i.MX6 DualLite. Which makes the SD track lengths around 4 inches long. We would like to run the SD interface at SDR12 speed (25MHz).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is 4 inches of track length acceptable for SD interface to work at 25MHz? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Selcuk&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2015 15:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD-Card-maximum-PCB-Track-Lenghts/m-p/425645#M64480</guid>
      <dc:creator>skuzu</dc:creator>
      <dc:date>2015-11-19T15:50:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 SD Card maximum PCB Track Lenghts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD-Card-maximum-PCB-Track-Lenghts/m-p/425646#M64481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Selcuk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;length is acceptable. SD Layout guidelines can be found on&lt;/P&gt;&lt;P&gt;sect.6 SD/MMC/SDIO Card and SPI interfaces, 5.3 Minimizing Reflections&lt;/P&gt;&lt;P&gt;AN4215 &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4215.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4215.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4215.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 01:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD-Card-maximum-PCB-Track-Lenghts/m-p/425646#M64481</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-20T01:45:31Z</dc:date>
    </item>
  </channel>
</rss>