<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Ethernet and U-boot Environment variables</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-and-U-boot-Environment-variables/m-p/425249#M64377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saida&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. seems dp83848 is already integrated on some i.MX6 boards, like fs-net PicoMODA9 board&lt;/P&gt;&lt;P&gt;2. lwip was in i.MX6 SDK, if you previously got it, then one can find it in sdk/lwip directory&lt;/P&gt;&lt;P&gt;&amp;nbsp; (also please find attached this part ).&lt;/P&gt;&lt;P&gt;3. this is defined in uboot/include/configs/&amp;nbsp; files, #define CONFIG_ENV_IS_IN_FLASH.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For example one can look at mx6sabre_common.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Nov 2015 01:38:43 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-11-20T01:38:43Z</dc:date>
    <item>
      <title>Ethernet and U-boot Environment variables</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-and-U-boot-Environment-variables/m-p/425248#M64376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;i.mx community&lt;/P&gt;&lt;P&gt;this is my come back after small gap and i hope every community members are fine&lt;/P&gt;&lt;P&gt;for my i.mx6 sabresd board&lt;/P&gt;&lt;P&gt;1) how to modify ethernet driver in u-boot for my phy dp83848 TI chip&lt;/P&gt;&lt;P&gt;2) how i can port open source lwip TCP/IP stack to my custom board (i am not using OS, i want to make it standalone embedded system) so that my directly uses stack protocols.&lt;/P&gt;&lt;P&gt;3) sabre board doesn't have nor flash, environment variables are stored in MMC flash but in my board i have NOR flash where u-boot is stored and i want to store env in flash what are the modifications i have to do in u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is my urgent requirement plz any one can give quick reply to me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Saida&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2015 05:25:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-and-U-boot-Environment-variables/m-p/425248#M64376</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-11-19T05:25:26Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet and U-boot Environment variables</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-and-U-boot-Environment-variables/m-p/425249#M64377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saida&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. seems dp83848 is already integrated on some i.MX6 boards, like fs-net PicoMODA9 board&lt;/P&gt;&lt;P&gt;2. lwip was in i.MX6 SDK, if you previously got it, then one can find it in sdk/lwip directory&lt;/P&gt;&lt;P&gt;&amp;nbsp; (also please find attached this part ).&lt;/P&gt;&lt;P&gt;3. this is defined in uboot/include/configs/&amp;nbsp; files, #define CONFIG_ENV_IS_IN_FLASH.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For example one can look at mx6sabre_common.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 01:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-and-U-boot-Environment-variables/m-p/425249#M64377</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-20T01:38:43Z</dc:date>
    </item>
  </channel>
</rss>