<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX233 PCB Design with BGA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-PCB-Design-with-BGA/m-p/175076#M6437</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;few years ago I designed a custom board with imx233(BGA package), the board is working flawlessly to this day. So, this is what I used&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-I prefer the layer order in the AN, but I used four layers "top route-GND-POWER/GROUND-bottom route" I had imx233(BGA), 2X 64MB micron DDRs in TSOP-66, GSM modem, audio amplifiers, FM reciever, accelerometer and GPS chips all on top-layer of a "2.1x3.2" dimentson.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- The impedance matching is not that critical if you keep the traces very short. I used trace/space of 5mil and I haven't actually controlled the impedance, but I kept the traces as short as possible (longest 33mm)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- as for the balls, I used a 0.35mm pads, to get easy routing with 5mil traces and four layers. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cheers!&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Oct 2012 08:25:23 GMT</pubDate>
    <dc:creator>danix</dc:creator>
    <dc:date>2012-10-02T08:25:23Z</dc:date>
    <item>
      <title>iMX233 PCB Design with BGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-PCB-Design-with-BGA/m-p/175075#M6436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am actually reviewing AN3989 and Gerbers 77066 of EVK to design my own board.&lt;/P&gt;&lt;P&gt;I have some question, first, EVK layer order is different from AN, what's better ?&lt;/P&gt;&lt;P&gt;I can't found information about impedance requirement between IMX and DDR,&lt;/P&gt;&lt;P&gt;EVK say 50ohm for 3mils (very thin !) and have 5.5mils trace on L1, this give around&lt;/P&gt;&lt;P&gt;35ohm, it is correct (particularly for two DDR chip) ?&lt;/P&gt;&lt;P&gt;Finally, BGA pad are 0.355mm on EVK, less than 0.43mm+/-0.06 from datasheet,&lt;/P&gt;&lt;P&gt;is it really safe regarding stress on solder joint ?&lt;/P&gt;&lt;P&gt;Thanks for your answer.&lt;/P&gt;&lt;P&gt;SeB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Oct 2011 15:20:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX233-PCB-Design-with-BGA/m-p/175075#M6436</guid>
      <dc:creator>Neoseb30</dc:creator>
      <dc:date>2011-10-10T15:20:58Z</dc:date>
    </item>
    <item>
      <title>Re: iMX233 PCB Design with BGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-PCB-Design-with-BGA/m-p/175076#M6437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;few years ago I designed a custom board with imx233(BGA package), the board is working flawlessly to this day. So, this is what I used&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-I prefer the layer order in the AN, but I used four layers "top route-GND-POWER/GROUND-bottom route" I had imx233(BGA), 2X 64MB micron DDRs in TSOP-66, GSM modem, audio amplifiers, FM reciever, accelerometer and GPS chips all on top-layer of a "2.1x3.2" dimentson.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- The impedance matching is not that critical if you keep the traces very short. I used trace/space of 5mil and I haven't actually controlled the impedance, but I kept the traces as short as possible (longest 33mm)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- as for the balls, I used a 0.35mm pads, to get easy routing with 5mil traces and four layers. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cheers!&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2012 08:25:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX233-PCB-Design-with-BGA/m-p/175076#M6437</guid>
      <dc:creator>danix</dc:creator>
      <dc:date>2012-10-02T08:25:23Z</dc:date>
    </item>
  </channel>
</rss>