<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLCD RGB Color problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LCD-RGB-Color-problem/m-p/425228#M64369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ours is imx6q processor in which we have integrated a LVDS 800x600 display in Linux 3.10.17 with Yocto .So we have set all the parameters&amp;nbsp; according to the Datasheet .In software we have configured all the parameters in linux/drivers/video/mxc/ldb.c and the RGB value setting and bits per pixel value have been set in linux/arch/arm/boot/dts/*.dtsi file.But image obtained was not proper and there is some RGB mismatch. Can any one please conform what could be the mistake when configuring the LVDS with 6-bit RGB each.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 08 Aug 2015 05:59:58 GMT</pubDate>
    <dc:creator>deepanrajanbara</dc:creator>
    <dc:date>2015-08-08T05:59:58Z</dc:date>
    <item>
      <title>LCD RGB Color problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-RGB-Color-problem/m-p/425228#M64369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ours is imx6q processor in which we have integrated a LVDS 800x600 display in Linux 3.10.17 with Yocto .So we have set all the parameters&amp;nbsp; according to the Datasheet .In software we have configured all the parameters in linux/drivers/video/mxc/ldb.c and the RGB value setting and bits per pixel value have been set in linux/arch/arm/boot/dts/*.dtsi file.But image obtained was not proper and there is some RGB mismatch. Can any one please conform what could be the mistake when configuring the LVDS with 6-bit RGB each.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Aug 2015 05:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-RGB-Color-problem/m-p/425228#M64369</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2015-08-08T05:59:58Z</dc:date>
    </item>
    <item>
      <title>Re: LCD RGB Color problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-RGB-Color-problem/m-p/425229#M64370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deepanraj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the following thread’s responses you could find useful information regarding LCDs configurations on 640x480 resolution on i.MX processors:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/253444"&gt;Configuring the resolution of the VGA to support 800x600 and 640x480&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 20:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-RGB-Color-problem/m-p/425229#M64370</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-08-11T20:27:47Z</dc:date>
    </item>
  </channel>
</rss>