<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx6 boardbring up in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425172#M64357</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are using 3.10.53 version&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2015 06:57:59 GMT</pubDate>
    <dc:creator>srinivasaporam</dc:creator>
    <dc:date>2015-06-24T06:57:59Z</dc:date>
    <item>
      <title>i.mx6 boardbring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425170#M64355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are working on i.mx6 customized board which has just come after assembly. we were trying to port OS into it by deploying the SD card image, Uboot etc as explained in the Yocto project.&lt;/P&gt;&lt;P&gt; but when we are powering on the board by putting sd card into the board. nothing is appearing on the monitor which is connected to board through HDMI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in order to check the correctness and validate our design, we also got evaluation board wandboard quad, for which we have deployed respective image to sd card and powered on the board by putting sd card. then display is coming on the monitor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, this has confirmed that we are missing something in our board. while designing the board we taken the references from wand board and as well as sabrelite.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for example, we have taken sd card and other peripheral connections ,schematic and made connections based on wandboard and for some other systems like hdmi, csi we have considered sabrelite reference deisgns.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; now, our query is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yocto project is specifying procedure deploying the image files to sd card for particular architecture. But,&amp;nbsp; can we create image files files for customized boards (like our case which is mixture of both wand board and sabrelite). How can we do that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 05:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425170#M64355</guid>
      <dc:creator>srinivasaporam</dc:creator>
      <dc:date>2015-06-24T05:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 boardbring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425171#M64356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Srinivasa Poram，&lt;/P&gt;&lt;P&gt;Which version BSP are you using?&lt;BR /&gt;Have a great day,&lt;BR /&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 06:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425171#M64356</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2015-06-24T06:45:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 boardbring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425172#M64357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are using 3.10.53 version&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 06:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425172#M64357</guid>
      <dc:creator>srinivasaporam</dc:creator>
      <dc:date>2015-06-24T06:57:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 boardbring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425173#M64358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Srinivasa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at attached documents, in particular Yocto Guide&lt;/P&gt;&lt;P&gt;sect.7 Creating a Custom Board Configuration and links&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95333"&gt;Task #10 - How to create a custom layer&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.imx6rex.com/software/how-to-add-support-for-a-custom-board-into-yocto/" title="http://www.imx6rex.com/software/how-to-add-support-for-a-custom-board-into-yocto/"&gt;How to add support of custom board into YOCTO - iMX6 Rex Module&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 11:46:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-boardbring-up/m-p/425173#M64358</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-24T11:46:29Z</dc:date>
    </item>
  </channel>
</rss>