<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Creating file in file system reg</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Creating-file-in-file-system-reg/m-p/425169#M64354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Execute this once the target is up:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cat /proc/version &amp;gt; running_kernel_version.txt&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jun 2015 16:18:52 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2015-06-04T16:18:52Z</dc:date>
    <item>
      <title>Creating file in file system reg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-file-in-file-system-reg/m-p/425168#M64353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hai ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to create one file which contains kernel version in file system.It will create automatically when the kernel build occured&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 06:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-file-in-file-system-reg/m-p/425168#M64353</guid>
      <dc:creator>sachusanal</dc:creator>
      <dc:date>2015-06-04T06:06:36Z</dc:date>
    </item>
    <item>
      <title>Re: Creating file in file system reg</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-file-in-file-system-reg/m-p/425169#M64354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Execute this once the target is up:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cat /proc/version &amp;gt; running_kernel_version.txt&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 16:18:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-file-in-file-system-reg/m-p/425169#M64354</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2015-06-04T16:18:52Z</dc:date>
    </item>
  </channel>
</rss>