<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックamd-gpu-bin-mx51 libGLESv2.so linking error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/amd-gpu-bin-mx51-libGLESv2-so-linking-error/m-p/425053#M64340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I have a RSB4210 board (i.MX536) from Advantech running Linux 2.6.35.3.&lt;/P&gt;&lt;P&gt;I am building Qt 5.5 using Ubuntu 14.04 rootfs and gcc-linaro-4.9-2015.05-x86_64_arm-linux-gnueabihf compilter.&lt;/P&gt;&lt;P&gt;I want to use EGLFS backend which requires OpenGL ES libraries.&lt;/P&gt;&lt;P&gt;I've downloaded amd-gpu-bin-mx51 (and unpacked to my rootfs) libraries from here:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="https://www.freescale.com/webapp/Download?colCode=IMX53_LINUX_1109_BSP_PATCH&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1298413274207729722207&amp;amp;Parent_pageType=product" rel="nofollow"&gt;https://www.freescale.com/webapp/Download?colCode=IMX53_LINUX_1109_BSP_PATCH&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;But when I try to configure Qt, I get the following error:&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `operator new[](unsigned int)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `__gnu_cxx::__exchange_and_add(int volatile*, int)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `__aeabi_atexit@CXXABI_ARM_1.3.3'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `std::string::assign(std::string const&amp;amp;)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `std::string::_Rep::_M_destroy(std::allocator&amp;lt;char&amp;gt; const&amp;amp;)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `std::string::resize(unsigned int, char)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `operator delete(void*)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;[... and lots of other undefined references]&lt;/P&gt;&lt;P&gt;collect2: error: ld returned 1 exit status&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that those libraries from amd-gpu-bin-mx51 archive are not compatible with new glibc from ubuntu 14.04.&lt;/P&gt;&lt;P&gt;Is there an updated version of those libraries? The version I found on Freescale site is from 2011.&lt;/P&gt;&lt;P&gt;Or is there a way to work around this error?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Sep 2015 20:32:58 GMT</pubDate>
    <dc:creator>vyacheslav_maty</dc:creator>
    <dc:date>2015-09-03T20:32:58Z</dc:date>
    <item>
      <title>amd-gpu-bin-mx51 libGLESv2.so linking error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/amd-gpu-bin-mx51-libGLESv2-so-linking-error/m-p/425053#M64340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I have a RSB4210 board (i.MX536) from Advantech running Linux 2.6.35.3.&lt;/P&gt;&lt;P&gt;I am building Qt 5.5 using Ubuntu 14.04 rootfs and gcc-linaro-4.9-2015.05-x86_64_arm-linux-gnueabihf compilter.&lt;/P&gt;&lt;P&gt;I want to use EGLFS backend which requires OpenGL ES libraries.&lt;/P&gt;&lt;P&gt;I've downloaded amd-gpu-bin-mx51 (and unpacked to my rootfs) libraries from here:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="https://www.freescale.com/webapp/Download?colCode=IMX53_LINUX_1109_BSP_PATCH&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1298413274207729722207&amp;amp;Parent_pageType=product" rel="nofollow"&gt;https://www.freescale.com/webapp/Download?colCode=IMX53_LINUX_1109_BSP_PATCH&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;But when I try to configure Qt, I get the following error:&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `operator new[](unsigned int)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `__gnu_cxx::__exchange_and_add(int volatile*, int)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `__aeabi_atexit@CXXABI_ARM_1.3.3'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `std::string::assign(std::string const&amp;amp;)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `std::string::_Rep::_M_destroy(std::allocator&amp;lt;char&amp;gt; const&amp;amp;)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `std::string::resize(unsigned int, char)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;...path/to/rootfs/usr/lib/libGLESv2.so: undefined reference to `operator delete(void*)@GLIBCXX_3.4'&lt;/P&gt;&lt;P&gt;[... and lots of other undefined references]&lt;/P&gt;&lt;P&gt;collect2: error: ld returned 1 exit status&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that those libraries from amd-gpu-bin-mx51 archive are not compatible with new glibc from ubuntu 14.04.&lt;/P&gt;&lt;P&gt;Is there an updated version of those libraries? The version I found on Freescale site is from 2011.&lt;/P&gt;&lt;P&gt;Or is there a way to work around this error?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 20:32:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/amd-gpu-bin-mx51-libGLESv2-so-linking-error/m-p/425053#M64340</guid>
      <dc:creator>vyacheslav_maty</dc:creator>
      <dc:date>2015-09-03T20:32:58Z</dc:date>
    </item>
    <item>
      <title>Re: amd-gpu-bin-mx51 libGLESv2.so linking error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/amd-gpu-bin-mx51-libGLESv2-so-linking-error/m-p/425054#M64341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;bump&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 12:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/amd-gpu-bin-mx51-libGLESv2-so-linking-error/m-p/425054#M64341</guid>
      <dc:creator>vyacheslav_maty</dc:creator>
      <dc:date>2015-09-08T12:42:11Z</dc:date>
    </item>
    <item>
      <title>Re: amd-gpu-bin-mx51 libGLESv2.so linking error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/amd-gpu-bin-mx51-libGLESv2-so-linking-error/m-p/425055#M64342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vyacheslav,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct!, those files are not compatible with latest ubuntu 14, and as far as I know there is no any upgrade on those AMD gpu binaries, also, kernel 2.6 is not possible to be compiled gcc 4.9. &lt;/P&gt;&lt;P&gt;You can contact AMD for support on it. Or try to use the Yocto community project for using amd gpu library and QT4 or QT5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 15:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/amd-gpu-bin-mx51-libGLESv2-so-linking-error/m-p/425055#M64342</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2015-09-17T15:24:52Z</dc:date>
    </item>
  </channel>
</rss>