<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic URGENT : Changing DRIVE STRENGTH of DDR3 (MR1) via MRS commands in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/URGENT-Changing-DRIVE-STRENGTH-of-DDR3-MR1-via-MRS-commands/m-p/424317#M64149</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As we are validating the DDR3 read and write burst, we could see failures in DQS output slew rate (SRQdiff) and data output slew rate (SRQ-se).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, we are thinking to change the drive strength of DDR3 through MRS commands (MR1 register : M5&amp;amp;M1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To enable/modify the DDR drive strength, we have modified the "flash_headers.S" from u-boot,&lt;/P&gt;&lt;P&gt;MXC_DCD_ITEM(75,MMDC_P0_BASE_ADDR + 0x01C, 0x00048031)&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;MXC_DCD_ITEM(75,MMDC_P0_BASE_ADDR + 0x01C, 0x00048011)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I'm not able to get any prints on tera term, its just completely hang.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone suggest on what to do for making DDR3 passing JEDEC standard and how to change the DDR drive strength for DDR3 and where &amp;amp; which file need to change .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: We have calibrated and written given calibrated data from DDR stress test tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;S.Titus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Sep 2015 13:14:06 GMT</pubDate>
    <dc:creator>titusstalin</dc:creator>
    <dc:date>2015-09-03T13:14:06Z</dc:date>
    <item>
      <title>URGENT : Changing DRIVE STRENGTH of DDR3 (MR1) via MRS commands</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/URGENT-Changing-DRIVE-STRENGTH-of-DDR3-MR1-via-MRS-commands/m-p/424317#M64149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As we are validating the DDR3 read and write burst, we could see failures in DQS output slew rate (SRQdiff) and data output slew rate (SRQ-se).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, we are thinking to change the drive strength of DDR3 through MRS commands (MR1 register : M5&amp;amp;M1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To enable/modify the DDR drive strength, we have modified the "flash_headers.S" from u-boot,&lt;/P&gt;&lt;P&gt;MXC_DCD_ITEM(75,MMDC_P0_BASE_ADDR + 0x01C, 0x00048031)&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;MXC_DCD_ITEM(75,MMDC_P0_BASE_ADDR + 0x01C, 0x00048011)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I'm not able to get any prints on tera term, its just completely hang.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone suggest on what to do for making DDR3 passing JEDEC standard and how to change the DDR drive strength for DDR3 and where &amp;amp; which file need to change .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: We have calibrated and written given calibrated data from DDR stress test tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;S.Titus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 13:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/URGENT-Changing-DRIVE-STRENGTH-of-DDR3-MR1-via-MRS-commands/m-p/424317#M64149</guid>
      <dc:creator>titusstalin</dc:creator>
      <dc:date>2015-09-03T13:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: URGENT : Changing DRIVE STRENGTH of DDR3 (MR1) via MRS commands</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/URGENT-Changing-DRIVE-STRENGTH-of-DDR3-MR1-via-MRS-commands/m-p/424318#M64150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;just one comment:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;usually DQS and DQ output slew rate are referring to the DRAM output slew rate. This is measured on a special testboad, but not in the system.&lt;/P&gt;&lt;P&gt;Even if this would be controller in this case I don't think it makes sense to do this measurement in the system environment. &lt;/P&gt;&lt;P&gt;The DRAM and Controller vendor have to ensure that their devices fulfill the Output specs.&lt;/P&gt;&lt;P&gt;Unforunatelly the Scope Compliance tools call the Tests "Read Tests", but these are Data output tests and are not to be performed in the system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can help you to do and understand your tests and settings, but I can not help you how to change the settings ..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hermann&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 18:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/URGENT-Changing-DRIVE-STRENGTH-of-DDR3-MR1-via-MRS-commands/m-p/424318#M64150</guid>
      <dc:creator>hermann_ruckerb</dc:creator>
      <dc:date>2015-09-03T18:13:55Z</dc:date>
    </item>
    <item>
      <title>Re: URGENT : Changing DRIVE STRENGTH of DDR3 (MR1) via MRS commands</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/URGENT-Changing-DRIVE-STRENGTH-of-DDR3-MR1-via-MRS-commands/m-p/424319#M64151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Titus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for DDR drive strength changing one needs to modify MR1 register&lt;/P&gt;&lt;P&gt;register MMDCx_MDSCR, CMD_BA=1 with CMD_ADDR (bits 31-16)&lt;/P&gt;&lt;P&gt;set to Definition Mode Register 1 (MR1) given in DDR3 datasheet,&lt;/P&gt;&lt;P&gt;for example for MT41K128M16JT :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="MR1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54764iD138F5EBD32F5865/image-size/large?v=v2&amp;amp;px=999" role="button" title="MR1.jpg" alt="MR1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so bits (M5, M1) will be bits (21,17) MMDCx_MDSCR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 01:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/URGENT-Changing-DRIVE-STRENGTH-of-DDR3-MR1-via-MRS-commands/m-p/424319#M64151</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-04T01:12:40Z</dc:date>
    </item>
  </channel>
</rss>