<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6SL MFG_TOOL can not load kernel image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-MFG-TOOL-can-not-load-kernel-image/m-p/424212#M64124</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xuebing,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry I got confused, is MFGTools able to finish without errors?, are you using a demo image or are you building it from source code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jul 2015 14:22:58 GMT</pubDate>
    <dc:creator>SergioSolis</dc:creator>
    <dc:date>2015-07-09T14:22:58Z</dc:date>
    <item>
      <title>iMX6SL MFG_TOOL can not load kernel image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-MFG-TOOL-can-not-load-kernel-image/m-p/424211#M64123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi iMX6 community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying iMX6 MFG_TOOL: imx-3.10.17-1.0.0-ga-mfg-tools. My board is based on iMX6SL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After I launch MfgTool2 on Windows7, and click &amp;lt;start&amp;gt; button, u-boot can be loaded. However, u-boot displays error message "Wrong Image Format for bootm command. ERROR: can't get kernel image!"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Detailed u-boot load is as below:&lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;Boot from USB for mfgtools&lt;/P&gt;&lt;P&gt;Use default environment for mfgtools&lt;/P&gt;&lt;P&gt;Run bootcmd_mfg: run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;Wrong Image Format for bootm command&lt;/P&gt;&lt;P&gt;ERROR: can't get kernel image!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv mfgtool_args &lt;/P&gt;&lt;P&gt;mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_&lt;/P&gt;&lt;P&gt;mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; md.w&amp;nbsp; 0x82000000 10&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;82000000: 0530 5619 be50 12e8 6e55 71e3 4800 2024&amp;nbsp;&amp;nbsp;&amp;nbsp; 0..VP...Un.q.H$ &lt;/P&gt;&lt;P&gt;82000010: 0080 0080 0080 0080 2708 dd52 0205 0002&amp;nbsp;&amp;nbsp;&amp;nbsp; .........'R.....&lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First 2 bytes at address 0x82000000 is 0530, while these 2 bytes of my uImage is 0527 (different from 0530).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After "mw.w 0x82000000 0527", then kernel can be loaded by "bootm ${loadaddr} - ${fdt_addr};"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea why the first byte of uImage is changed? Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-- Xuebing Wang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 11:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-MFG-TOOL-can-not-load-kernel-image/m-p/424211#M64123</guid>
      <dc:creator>xuebingwang</dc:creator>
      <dc:date>2015-06-03T11:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SL MFG_TOOL can not load kernel image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-MFG-TOOL-can-not-load-kernel-image/m-p/424212#M64124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xuebing,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry I got confused, is MFGTools able to finish without errors?, are you using a demo image or are you building it from source code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2015 14:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SL-MFG-TOOL-can-not-load-kernel-image/m-p/424212#M64124</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2015-07-09T14:22:58Z</dc:date>
    </item>
  </channel>
</rss>