<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Debugging Linux Kernel over JTAG with J-Link</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424125#M64104</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We took JTAG off of our board pretty early on in the dev cycle, so I can't easily verify for you.&amp;nbsp; But, one thing you can try is breaking into u-boot, and then attaching at that point.&amp;nbsp; If you _can_ attach to u-boot, but can't attach to linux, then I'd guess it's either some necessary clock which Linux is either disabling, or changing frequency.&amp;nbsp; Or, it might be something in the pinmux which is changing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Dec 2017 17:16:32 GMT</pubDate>
    <dc:creator>skrap</dc:creator>
    <dc:date>2017-12-09T17:16:32Z</dc:date>
    <item>
      <title>Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424120#M64099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We've been working through getting a working setup for debugging the linux kernel via JTAG, using Segger's J-Link.&amp;nbsp; There's a few hints on this forum and elsewhere, but not a complete guide, so here's what works for us:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First: if you just go and try debugging the kernel, you'll probably find that you either:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;can't connect at all once linux has booted, or&lt;/LI&gt;&lt;LI&gt;if you connect at u-boot, and then let linux load, you get disconnected around the time that init runs, or&lt;/LI&gt;&lt;LI&gt;if you get lucky and manage to connect when linux is running, you get disconnected shortly afterwards.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue is caused by linux going into a low power idle state.&amp;nbsp; In this state, linux will gate the ARM clock domain, causing the JTAG to lose connection whenever the OS is executing the idle task. There are two ways around this. The first is less invasive, but slightly more limited.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H1&gt;Method 1 (easy method): Disable 'clock off' wait state in the cpuidle driver&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the IMX6 you can disable the clock off wait state through sysfs. Navigate to the cpuidle driver for the cpu (cpu0 in this case as we are on the solo lite). &lt;/P&gt;&lt;P class="panel code"&gt;&lt;/P&gt;&lt;DIV class="panelContent codeContent"&gt;&lt;DIV&gt;&lt;DIV class="syntaxhighlighter nogutter java"&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD class="code"&gt;&lt;DIV class="container" title="Hint: double-click to select code"&gt;&lt;DIV class="number1 alt2 line index0"&gt;&lt;CODE class="plain java"&gt;cd /sys/devices/system/cpu/cpu0/cpuidle/state1&lt;/CODE&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="number2 alt1 line index1"&gt;&lt;CODE class="plain java"&gt;cat desc&lt;/CODE&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;The output of 'cat desc' should be 'Clock off'. If this is not the case, go up a folder and check the other states until you find the one with the 'Clock off' desc. Now, you simply need to disable this wait state&lt;/P&gt;&lt;P class="panel code"&gt;&lt;/P&gt;&lt;DIV class="panelContent codeContent"&gt;&lt;DIV&gt;&lt;DIV class="syntaxhighlighter nogutter java"&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD class="code"&gt;&lt;DIV class="container" title="Hint: double-click to select code"&gt;&lt;DIV class="number1 alt2 line index0"&gt;&lt;CODE class="plain java"&gt;echo &lt;/CODE&gt;&lt;CODE class="value java"&gt;1&lt;/CODE&gt; &lt;CODE class="plain java"&gt;&amp;gt; disable&lt;/CODE&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;Now you should be able to attach with JTAG and debug to your heart's content.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H1&gt;Method 2 (harder method): Disable gating of the ARM clock domain in the source&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The above method is good for most cases of debugging, unless something needs to be debugged during startup. In this case you will need to modify the source to stop the IMX from ever gating the ARM clock domain. You can apply the following patch to disable the clock gating.&lt;/P&gt;&lt;P class="panel code"&gt;&lt;/P&gt;&lt;DIV class="panelContent codeContent"&gt;&lt;DIV&gt;&lt;DIV class="syntaxhighlighter diff nogutter"&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD class="code"&gt;&lt;DIV class="container" title="Hint: double-click to select code"&gt;&lt;DIV class="number1 alt2 line index0"&gt;&lt;CODE class="diff plain"&gt;diff --git a/arch/arm/mach-imx/pm-imx6.c b/arch/arm/mach-imx/pm-imx6.c&lt;/CODE&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="number2 alt1 line index1"&gt;&lt;CODE class="diff plain"&gt;index e1a45e2..feadccb 100644&lt;/CODE&gt;&lt;/P&gt;&lt;P class="number3 index2 alt2 line"&gt;&lt;CODE class="color2 diff"&gt;--- a/arch/arm/mach-imx/pm-imx6.c&lt;/CODE&gt;&lt;/P&gt;&lt;P class="index3 number4 alt1 line"&gt;&lt;CODE class="color2 diff"&gt;+++ b/arch/arm/mach-imx/pm-imx6.c&lt;/CODE&gt;&lt;/P&gt;&lt;P class="index4 alt2 line number5"&gt;&lt;CODE class="diff plain"&gt;@@ -552,8 +552,8 @@ int imx6q_set_lpm(enum mxc_cpu_pwr_mode mode)&lt;/CODE&gt;&lt;/P&gt;&lt;P class="index5 alt1 line number6"&gt;&lt;CODE class="spaces diff"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;CODE class="color1 diff"&gt;case WAIT_CLOCKED:&lt;/CODE&gt;&lt;/P&gt;&lt;P class="number7 alt2 index6 line"&gt;&lt;CODE class="spaces diff"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;CODE class="color1 diff"&gt;break;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="index7 number8 alt1 line"&gt;&lt;CODE class="spaces diff"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;CODE class="color1 diff"&gt;case WAIT_UNCLOCKED:&lt;/CODE&gt;&lt;/P&gt;&lt;P class="number9 alt2 line index8"&gt;&lt;CODE class="diff comments"&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; val |= 0x1 &amp;lt;&amp;lt; BP_CLPCR_LPM;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="alt1 line index9 number10"&gt;&lt;CODE class="diff comments"&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; val |= BM_CLPCR_ARM_CLK_DIS_ON_LPM;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="number13 alt2 line index12"&gt;&lt;CODE class="spaces diff"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;CODE class="color1 diff"&gt;break;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="index13 number14 alt1 line"&gt;&lt;CODE class="spaces diff"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;CODE class="color1 diff"&gt;case STOP_POWER_ON:&lt;/CODE&gt;&lt;/P&gt;&lt;P class="index14 number15 alt2 line"&gt;&lt;CODE class="spaces diff"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;CODE class="color1 diff"&gt;val |= 0x2 &amp;lt;&amp;lt; BP_CLPCR_LPM;&lt;/CODE&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;H1&gt;&lt;/H1&gt;&lt;H1&gt;J-Link setup&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have been using the Segger J-Link to debug ARM platforms from a linux host. Download the Segger J-Link tools for Linux from the &lt;A class="external-link" href="https://www.segger.com/jlink-software.html" rel="nofollow" target="_blank"&gt;Segger website&lt;/A&gt;. After you have done one of the two above methods you can now attach the J-Link GDB server. Note that by default your user wont have permissions to access the J-Link USB device. You can either setup a udev rule to set the permissions properly, or simply run the gdb server as root. We will do the latter as we are lazy. Note the noir and noreset options. noir will not init the working register and noreset won't reset the cpu core. See the J-Link documentation included with the download for more info.&lt;/P&gt;&lt;P class="panel code"&gt;&lt;/P&gt;&lt;DIV class="panelContent codeContent"&gt;&lt;DIV&gt;&lt;DIV class="syntaxhighlighter nogutter java"&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD class="code"&gt;&lt;DIV class="container" title="Hint: double-click to select code"&gt;&lt;DIV class="number1 alt2 line index0"&gt;&lt;CODE class="plain java"&gt;sudo ./JLinkGDBServer -&lt;/CODE&gt;&lt;CODE class="keyword java"&gt;if&lt;/CODE&gt; &lt;CODE class="plain java"&gt;JTAG -endian little -device MCIMX6L8 -select USB -noir -noreset&lt;/CODE&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;H1&gt;&lt;/H1&gt;&lt;H1&gt;Helpful kernel configuration options for debugging&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before diving right into debugging, note there are some useful kernel configuration options that will make your life a lot easier. Below is a list of kernel configuration options you should set:&lt;/P&gt;&lt;P class="panel code"&gt;&lt;/P&gt;&lt;DIV class="panelContent codeContent"&gt;&lt;DIV&gt;&lt;DIV class="syntaxhighlighter nogutter java"&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD class="code"&gt;&lt;DIV class="container" title="Hint: double-click to select code"&gt;&lt;DIV class="number1 alt2 line index0"&gt;&lt;CODE class="plain java"&gt;CONFIG_DEBUG_INFO=y # &lt;/CODE&gt;&lt;CODE class="keyword java"&gt;this&lt;/CODE&gt; &lt;CODE class="plain java"&gt;will compile in debugging symbols and info&lt;/CODE&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;H1&gt;&lt;/H1&gt;&lt;H1&gt;GDB client connection and debugging!&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, with a GDB server running that is connected to your target, you can connect with a GDB client. Note that you can point GDB to your linux binary for the debugging information. Also, you should use your cross compile GDB for this target. If you are using the Yocto Poky SDK (as we are), you can simply source the SDK and use '$GDB' in place of gdb-[CROSS-COMPILE] below. Note that [CROSS-COMPILE] should be replaced with your proper cross compile tuple (e.g. gdb-arm-linux-eabi).&lt;/P&gt;&lt;P class="container" title="Hint: double-click to select code"&gt;&lt;/P&gt;&lt;DIV class="number1 alt2 line index0"&gt;&lt;CODE class="plain java"&gt;$ gdb-[CROSS-COMPILE] /path/to/linux/build/vmlinux&lt;/CODE&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="number2 alt1 line index1"&gt;&lt;CODE class="plain java"&gt;(gdb) target remote localhost:&lt;/CODE&gt;&lt;CODE class="value java"&gt;2331&lt;/CODE&gt;&lt;/P&gt;&lt;P class="number2 alt1 line index1"&gt;&lt;/P&gt;&lt;P class="number2 alt1 line index1"&gt;Enjoy your debugging session!&amp;nbsp; Any questions or comments, please post them below.&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Sep 2015 13:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424120#M64099</guid>
      <dc:creator>jonahpetri</dc:creator>
      <dc:date>2015-09-30T13:29:04Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424121#M64100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for putting the details up. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Oct 2015 23:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424121#M64100</guid>
      <dc:creator>sanjaymishra</dc:creator>
      <dc:date>2015-10-18T23:45:24Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424122#M64101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One follow-up on this: the i.MX7 has a further low-power state beyond "Clock off", so you should probably do something like this for "method 1" above:&lt;/P&gt;&lt;PRE&gt;#!/bin/sh
for i in /sys/devices/system/cpu/cpu*/cpuidle/state[123456789]/disable; do 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; echo 1 &amp;gt; $i
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; echo $i
done&lt;/PRE&gt;&lt;P&gt;The [123456789] above is just trying to avoid state0, which is WFI and is OK for JTAG debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to debug using "method 2" above, the easiest thing may be to just turn off CONFIG_CPU_IDLE in your kernel config.&amp;nbsp; I haven't verified, but that should do the trick.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 20:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424122#M64101</guid>
      <dc:creator>skrap</dc:creator>
      <dc:date>2017-01-20T20:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424123#M64102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just a quick node, in case you are working with an EVK for the IMX6UL, don't forget to disable the sai2 in the device tree, which pinmuxes away the jtag in favor of SAI pins.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 08:50:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424123#M64102</guid>
      <dc:creator>arnoutdiels</dc:creator>
      <dc:date>2017-06-01T08:50:02Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424124#M64103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The setup doesn't appear to work on iMX7D, Sabre board, with default Linux &amp;amp; image as provided by NXP, when you try to connect to the M4 core.&amp;nbsp; The entire SoC, or A7 core(s), get reset, when J-Link tries to connect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 17:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424124#M64103</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2017-12-09T17:06:32Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424125#M64104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We took JTAG off of our board pretty early on in the dev cycle, so I can't easily verify for you.&amp;nbsp; But, one thing you can try is breaking into u-boot, and then attaching at that point.&amp;nbsp; If you _can_ attach to u-boot, but can't attach to linux, then I'd guess it's either some necessary clock which Linux is either disabling, or changing frequency.&amp;nbsp; Or, it might be something in the pinmux which is changing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 17:16:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424125#M64104</guid>
      <dc:creator>skrap</dc:creator>
      <dc:date>2017-12-09T17:16:32Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424126#M64105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well yea, with u-boot it's not an issue, sorry I should have mentioned it.&lt;/P&gt;&lt;P&gt;It is Linux magic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Already removed disabling of unused clocks,&amp;nbsp; halt instructions (wfi), and cpu frequency set to off (all from linux boot command line). So that is all similar&amp;nbsp; / same as you have found above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the thing still resets ... Is there some hardware protection mechanism which can get enabled in software, which would exclude J-Link connection to the M4 core, and reset the SoC when trying?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can connect fine to A7_0 core.. halt/go Linux. But cannot access M4 SCR register from debugger, to say, enable M4 this way.&amp;nbsp; (And any attempt to then connect to M4 resets the entire thing, sorry repeating).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Urg.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 17:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424126#M64105</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2017-12-09T17:55:26Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424127#M64106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There's a hardware watchdog... that might do it, but under normal configurations it's either disabled or ticks every 10 seconds or so...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 18:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424127#M64106</guid>
      <dc:creator>skrap</dc:creator>
      <dc:date>2017-12-09T18:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424128#M64107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've not tried to use the M4, so I am not going to be of too much help.&amp;nbsp; I do note that there are M4-specific J-Link configurations here: &lt;A class="jivelink8" href="https://wiki.segger.com/IMX7D" title="https://wiki.segger.com/IMX7D"&gt;https://wiki.segger.com/IMX7D&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 18:37:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424128#M64107</guid>
      <dc:creator>skrap</dc:creator>
      <dc:date>2017-12-09T18:37:08Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424129#M64108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yea I've set nowatchdog parameter too, and even proceeded to remove all from kernel config &amp;amp; rebuild ..&lt;/P&gt;&lt;P&gt;The system resets way too quick for 10 secs.. it's almost immediately on connect attempt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 18:45:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424129#M64108</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2017-12-09T18:45:38Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424130#M64109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yea thanks, I think i've learned every word of that connect script by now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But may be i need to double check if it's being used at all, so thanks for pointing it out&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 18:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424130#M64109</guid>
      <dc:creator>dry</dc:creator>
      <dc:date>2017-12-09T18:48:18Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Linux Kernel over JTAG with J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424131#M64110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All right, best of luck!&amp;nbsp; If I have any other ideas, I'll post them here.&amp;nbsp; I hope if you find a solution you'll also add it!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 18:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-Linux-Kernel-over-JTAG-with-J-Link/m-p/424131#M64110</guid>
      <dc:creator>skrap</dc:creator>
      <dc:date>2017-12-09T18:50:15Z</dc:date>
    </item>
  </channel>
</rss>