<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: uboot ldo_bypass in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uboot-ldo-bypass/m-p/424011#M64067</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Qiang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;are you able to boot with ldo enabled - using xxx-imx6q-sabresd-ldo.dtb ?&lt;/P&gt;&lt;P&gt;If yes - then probably you are having PMIC problems - please check&lt;/P&gt;&lt;P&gt;that it can be controlled by processor.&lt;/P&gt;&lt;P&gt;If not - then probably you have ddr errors and one needs to run DDR test&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="32294" data-containertype="2020" data-content-finding="Community" data-objectid="96412" data-objecttype="102" href="https://community.nxp.com/docs/DOC-96412"&gt;https://community.freescale.com/docs/DOC-96412&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and update memory settings. Recommended to use FSL BSP&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow" target="_blank"&gt;L3.10.53_1.1.0_iMX6QDLS_Bundle&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2015 14:30:35 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-06-24T14:30:35Z</dc:date>
    <item>
      <title>uboot ldo_bypass</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-ldo-bypass/m-p/424010#M64066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;uboot:2014&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;kernel:3.10.53&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;UBOOT LOG:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;No panel detected: default to Hannstar-XGA&lt;/P&gt;&lt;P&gt;Display: Hannstar-XGA (1024x768)&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Found PFUZE100 deviceid=10,revid=11&lt;/P&gt;&lt;P&gt;mmc1 is current device&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; FEC [PRIME]&lt;/P&gt;&lt;P&gt;Normal Boot&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;mmc1 is current device&lt;/P&gt;&lt;P&gt;reading boot.scr&lt;/P&gt;&lt;P&gt;** Unable to read file boot.scr **&lt;/P&gt;&lt;P&gt;reading zImage&lt;/P&gt;&lt;P&gt;5545424 bytes read in 257 ms (20.6 MiB/s)&lt;/P&gt;&lt;P&gt;Booting from mmc ...&lt;/P&gt;&lt;P&gt;reading imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;49575 bytes read in 18 ms (2.6 MiB/s)&lt;/P&gt;&lt;P&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x549dd0 ]&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 18000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x18000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Using Device Tree in place at 18000000, end 1800f1a6&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;switch to ldo_bypass mode!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;(这里的ldo_bypass作用是什么，并且还是用到了i2c,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;如果我把UBOOT里的设置ldo_bypass删除，可以正常引导内核，内核会卡在Galcore version 5.0.11.25762这句话)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;附件是正常的log&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336767"&gt;normallog.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 02:47:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-ldo-bypass/m-p/424010#M64066</guid>
      <dc:creator>强王</dc:creator>
      <dc:date>2015-06-24T02:47:19Z</dc:date>
    </item>
    <item>
      <title>Re: uboot ldo_bypass</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-ldo-bypass/m-p/424011#M64067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Qiang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;are you able to boot with ldo enabled - using xxx-imx6q-sabresd-ldo.dtb ?&lt;/P&gt;&lt;P&gt;If yes - then probably you are having PMIC problems - please check&lt;/P&gt;&lt;P&gt;that it can be controlled by processor.&lt;/P&gt;&lt;P&gt;If not - then probably you have ddr errors and one needs to run DDR test&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="32294" data-containertype="2020" data-content-finding="Community" data-objectid="96412" data-objecttype="102" href="https://community.nxp.com/docs/DOC-96412"&gt;https://community.freescale.com/docs/DOC-96412&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and update memory settings. Recommended to use FSL BSP&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow" target="_blank"&gt;L3.10.53_1.1.0_iMX6QDLS_Bundle&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 14:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-ldo-bypass/m-p/424011#M64067</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-24T14:30:35Z</dc:date>
    </item>
  </channel>
</rss>