<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Hello, in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423760#M64010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the i.MX6 it is able to handle up to 4 cameras,&amp;nbsp; but this four cameras are using the CSI interface which it is a digital interface, I do not quite understand that you are mention Analog cameras, that can no be connect to the CSI port directly you need to add some kind of encoder to do so.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jun 2015 17:01:26 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2015-06-03T17:01:26Z</dc:date>
    <item>
      <title>Hello,</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423759#M64009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can i use 4 analog camera's with Imx6 Quad processor and stream them at a time.?&lt;/P&gt;&lt;P&gt;There are 4 CSI signals available. but how can i use them to connect 4 camera's.&lt;/P&gt;&lt;P&gt;If i do so, Can i able to stream them at the same time?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 13:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423759#M64009</guid>
      <dc:creator>raghavendrajama</dc:creator>
      <dc:date>2015-06-03T13:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: Hello,</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423760#M64010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the i.MX6 it is able to handle up to 4 cameras,&amp;nbsp; but this four cameras are using the CSI interface which it is a digital interface, I do not quite understand that you are mention Analog cameras, that can no be connect to the CSI port directly you need to add some kind of encoder to do so.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 17:01:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423760#M64010</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2015-06-03T17:01:26Z</dc:date>
    </item>
    <item>
      <title>Re: Hello,</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423761#M64011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello James,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;Yeah i thought of using ADV7280-M video decoders in between analog camera and the processor which will convert camera output to CSI.&lt;/P&gt;&lt;P&gt;My question is, can i able to stream all of them simultaneously? If yes, How can i take use of 4 CSI signals to achieve my requirement.&lt;/P&gt;&lt;P&gt;I mean i think to stream all the camera at the same time we need 4 CSI signals with 4 video decoders and 2 I2C. Please correct me if my understanding is wrong. Else suggest me with the new mode of connecting CSI signals to achieve this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 06:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423761#M64011</guid>
      <dc:creator>raghavendrajama</dc:creator>
      <dc:date>2015-06-04T06:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: Hello,</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423762#M64012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes you are correct, you need to have 4 CSI to achieve to stream simultaneously, and the i.MX6 only has 2. but one of them can be used as CSI-Mipi which allows to have the four cameras. So if you can use a video decoder to provide MIPI then you can do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2015 15:15:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hello/m-p/423762#M64012</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2015-06-10T15:15:01Z</dc:date>
    </item>
  </channel>
</rss>