<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423637#M63981</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;YESSSSS, I DID IT!!!!!!! IT WORKS!!!!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is how I solved my problem:&lt;BR /&gt;1. I had to activate the GPIOs to override the Fuses on 0x450 by setting BOOT_MODE to '01' (not really nessesary but helpful to play with fuses).&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Note to me: I think BOOT_MODE '10' is better for my purposes -&amp;gt; test it later.&lt;/P&gt;&lt;P&gt;2. Set "DDR Memory Map default config" in BOOT_CFG3 to '10' with the now active GPIOs. This activates interleaving mode for LPDDR2 to achieve a continous memory.&lt;/P&gt;&lt;P&gt;3. Change the Script-Aid:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The memory doesn't have two chip-selects. Although there are two CS-Pins, only one is active!&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Activate Interleaving mode&lt;/P&gt;&lt;P&gt;4. Change RAM-Size calculation in board specific C-File for U-Boot: The function "imx_ddr_size()" ignores two-channel-mode. So you have to set:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; gd-&amp;gt;ram_size = (imx_ddr_size()*2); //imx_ddr_size() ignores two channel mode. So double the size here! (!!!!!quick and dirty code!!!!!)&lt;/P&gt;&lt;P&gt;5. In device tree set the memory to a start-address of 0x10000000 (Base Address of MMDC0) and the range to 0x40000000 (1GiB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I remember, this was all I had to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps someone else, too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 May 2015 14:23:58 GMT</pubDate>
    <dc:creator>steffendoster</dc:creator>
    <dc:date>2015-05-28T14:23:58Z</dc:date>
    <item>
      <title>Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423630#M63974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm developing on a custom i.MX6Q-Board and we want to use a 2-Channel LPDDR2 configuration with two Micron MT42L128M32D1TK chips (512MB per chip).&lt;/P&gt;&lt;P&gt;But I'm nearly running mad with this because either u-boot shows only the half size of the RAM, crashes at RAM-calculation or doesn't even start. Oh, and I forgot the fourth case: I can even start Linux and everything tells me that the system now has 1GB, but I can't believe that because my system crashes when I test the RAM with&lt;/P&gt;&lt;P&gt;[CODE]&lt;/P&gt;&lt;P&gt;memtester 300 1&lt;/P&gt;&lt;P&gt;[/CODE]&lt;/P&gt;&lt;P&gt;I also think this is the reason why I can see the login-screen, but X-Server crashes when I try to login.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Short summary of my environment:&lt;/P&gt;&lt;P&gt;Debugger:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Trace32&lt;/P&gt;&lt;P&gt;Bootloader:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; U-Boot 2015.01&lt;/P&gt;&lt;P&gt;Boot-Device:&amp;nbsp;&amp;nbsp; SD-Card&lt;/P&gt;&lt;P&gt;Linux:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.19&lt;/P&gt;&lt;P&gt;Distribution:&amp;nbsp;&amp;nbsp;&amp;nbsp; Debian 8&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope, the connections between CPU and RAM are OK. I attached the &lt;STRONG&gt;schematic&lt;/STRONG&gt; in a pdf-file.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used the LPDDR2 Script Aid to get a somehow working configuration. I think everything is adjusted correctly, but if I use it the way it is now configured, U-Boot and Linux tell me that there are only 512MB RAM.&lt;/P&gt;&lt;P&gt;I also tried to set "Number of Chip Selects used per Channel" to 2, but this already crashes at boot of u-boot.&lt;/P&gt;&lt;P&gt;The resulting .cfg-file is &lt;STRONG&gt;sie_mx6q_ScriptAid.cfg.&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to configure a .cfg-file for U-Boot by my own. With this, the i.MX6 "thinks" it has 1GB of Memory and even boots to Login-Screen, but crashes on memtester (see above).&lt;/P&gt;&lt;P&gt;My own try is in &lt;STRONG&gt;sie_mx6q.cfg&lt;/STRONG&gt;.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What am I doing wrong? Or what didn't I understood?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you need further information?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336960"&gt;sie_mx6q.cfg.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336960"&gt;sie_mx6q-ScriptAid.cfg.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 10:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423630#M63974</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2015-05-12T10:02:12Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423631#M63975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steffan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; We are also facing similar issues in our custom board, in our case the part number is MT42L128M64D2 instead of&amp;nbsp; two MT42L128M32D1TK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"I tried to configure a .cfg-file for U-Boot by my own. With this, the i.MX6 "thinks" it has 1GB of Memory and even boots to Login-Screen, but crashes on memtester"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt; Can you provide a detailed boot-log for the above?&lt;/P&gt;&lt;P&gt; What is the maximum amount of memory you were able to test using memtester without getting the system to crash? We were able to get 130 MB :smileysad: above that system crashes.&lt;/P&gt;&lt;P&gt; Kindly provide the output of &lt;EM&gt;cat /proc/meminfo&lt;/EM&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 14:49:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423631#M63975</guid>
      <dc:creator>vijaikumar</dc:creator>
      <dc:date>2015-05-13T14:49:00Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423632#M63976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two cases:&lt;/P&gt;&lt;P&gt;1. RAM configured with script-aid:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN style="text-decoration: underline;"&gt;Crashes even with 100MB (throws some Kernel Messages of different types)&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; proc/meminfo:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;MemTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 500232 kB&lt;/P&gt;&lt;P&gt;MemFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 351900 kB&lt;/P&gt;&lt;P&gt;MemAvailable:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 420404 kB&lt;/P&gt;&lt;P&gt;Buffers:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 13968 kB&lt;/P&gt;&lt;P&gt;Cached:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 64872 kB&lt;/P&gt;&lt;P&gt;SwapCached:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Active:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 79892 kB&lt;/P&gt;&lt;P&gt;Inactive:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 41976 kB&lt;/P&gt;&lt;P&gt;Active(anon):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 43320 kB&lt;/P&gt;&lt;P&gt;Inactive(anon):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 6720 kB&lt;/P&gt;&lt;P&gt;Active(file):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 36572 kB&lt;/P&gt;&lt;P&gt;Inactive(file):&amp;nbsp;&amp;nbsp;&amp;nbsp; 35256 kB&lt;/P&gt;&lt;P&gt;Unevictable:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Mlocked:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;HighTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;HighFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;LowTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 500232 kB&lt;/P&gt;&lt;P&gt;LowFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 351900 kB&lt;/P&gt;&lt;P&gt;SwapTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;SwapFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Dirty:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16 kB&lt;/P&gt;&lt;P&gt;Writeback:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;AnonPages:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 43028 kB&lt;/P&gt;&lt;P&gt;Mapped:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 35328 kB&lt;/P&gt;&lt;P&gt;Shmem:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7016 kB&lt;/P&gt;&lt;P&gt;Slab:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 15988 kB&lt;/P&gt;&lt;P&gt;SReclaimable:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 8040 kB&lt;/P&gt;&lt;P&gt;SUnreclaim:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7948 kB&lt;/P&gt;&lt;P&gt;KernelStack:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 712 kB&lt;/P&gt;&lt;P&gt;PageTables:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 600 kB&lt;/P&gt;&lt;P&gt;NFS_Unstable:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Bounce:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;WritebackTmp:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;CommitLimit:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 250116 kB&lt;/P&gt;&lt;P&gt;Committed_AS:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 89284 kB&lt;/P&gt;&lt;P&gt;VmallocTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp; 1548288 kB&lt;/P&gt;&lt;P&gt;VmallocUsed:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5532 kB&lt;/P&gt;&lt;P&gt;VmallocChunk:&amp;nbsp;&amp;nbsp;&amp;nbsp; 1361448 kB&lt;/P&gt;&lt;P&gt;CmaTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16384 kB&lt;/P&gt;&lt;P&gt;CmaFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 11876 kB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. RAM configured somehow by myself:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN style="text-decoration: underline;"&gt;Crashes with 220MB. Until then it seems to work fine.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; proc/meminfo:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;MemTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1020012 kB&lt;/P&gt;&lt;P&gt;MemFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 868568 kB&lt;/P&gt;&lt;P&gt;MemAvailable:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 933736 kB&lt;/P&gt;&lt;P&gt;Buffers:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 14020 kB&lt;/P&gt;&lt;P&gt;Cached:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 67076 kB&lt;/P&gt;&lt;P&gt;SwapCached:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Active:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 79464 kB&lt;/P&gt;&lt;P&gt;Inactive:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 44540 kB&lt;/P&gt;&lt;P&gt;Active(anon):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 43200 kB&lt;/P&gt;&lt;P&gt;Inactive(anon):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 9000 kB&lt;/P&gt;&lt;P&gt;Active(file):&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 36264 kB&lt;/P&gt;&lt;P&gt;Inactive(file):&amp;nbsp;&amp;nbsp;&amp;nbsp; 35540 kB&lt;/P&gt;&lt;P&gt;Unevictable:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Mlocked:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;HighTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;HighFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;LowTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1020012 kB&lt;/P&gt;&lt;P&gt;LowFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 868568 kB&lt;/P&gt;&lt;P&gt;SwapTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;SwapFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Dirty:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Writeback:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;AnonPages:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 42840 kB&lt;/P&gt;&lt;P&gt;Mapped:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 35020 kB&lt;/P&gt;&lt;P&gt;Shmem:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 9296 kB&lt;/P&gt;&lt;P&gt;Slab:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 15940 kB&lt;/P&gt;&lt;P&gt;SReclaimable:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7928 kB&lt;/P&gt;&lt;P&gt;SUnreclaim:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 8012 kB&lt;/P&gt;&lt;P&gt;KernelStack:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 688 kB&lt;/P&gt;&lt;P&gt;PageTables:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 588 kB&lt;/P&gt;&lt;P&gt;NFS_Unstable:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;Bounce:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;WritebackTmp:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 kB&lt;/P&gt;&lt;P&gt;CommitLimit:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 510004 kB&lt;/P&gt;&lt;P&gt;Committed_AS:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 91932 kB&lt;/P&gt;&lt;P&gt;VmallocTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp; 1024000 kB&lt;/P&gt;&lt;P&gt;VmallocUsed:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5532 kB&lt;/P&gt;&lt;P&gt;VmallocChunk:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 837176 kB&lt;/P&gt;&lt;P&gt;CmaTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16384 kB&lt;/P&gt;&lt;P&gt;CmaFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 11876 kB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2015 09:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423632#M63976</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2015-05-18T09:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423633#M63977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steffen,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Have you calibrated the DDR for your board. If not can you use DDR Stress test to do a read and write calibration and see the result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Vijai Kumar K &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 11:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423633#M63977</guid>
      <dc:creator>vijaikumar</dc:creator>
      <dc:date>2015-05-22T11:23:06Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423634#M63978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to start the stress tester without any problems. It gave me some calibration values (0x403A383B) which are close to the default values (0x40404040) of the script-aid. due to the big distance to failure-values I kept the default values even if they are not optimal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the meantime I made another observation:&lt;/P&gt;&lt;P&gt;I read the RAM in u-boot using md. And this indicates me, that the RAM seems to be repeated every 512MiB.&lt;/P&gt;&lt;P&gt;By this way, everytime I try to write into the "upper" 512MiB it writes into the "lower" 512MiB. And this is often the place where the Kernel and other important things reside. This seems to be the reason, Linux crashes on trying "memtester 300 1".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also think this may be an error caused by wrong fuses, because "DDR Memory Map default config" is set to 0x00 in my fuses (see attached fuse-values) and this should be 0x01 or 0x10.&lt;/P&gt;&lt;P&gt;And this leads to another problem of mine:&lt;BR /&gt;How do I activate the GPIOs for overwriting the Fuses. I attached some DIP-Switches to the relevant EIM-Pads and I switched to BOOT_MODE[1:0] = 0b10. As you can see, BT_FUSE_SEL is set to 0. I think this must be enough to activate the external GPIOs for booting.&lt;/P&gt;&lt;P&gt;But I thought I now can see the Values of the GPIOs in Register 0x450. Where can I see the settings I made? Or what else do I have to set?&lt;/P&gt;&lt;P&gt;BOOT_MODE_0 = Pad C12, BOOT_MODE_1 = Pad F12 is correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 12:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423634#M63978</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2015-05-26T12:46:25Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423635#M63979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class="j-post-author"&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/people/steffendoster"&gt;steffendoster&lt;/A&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It is now evident that we are facing the same issue with our boards. I have started a discussion in the following location. &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/355364"&gt;Failed to execute /init (error -8) during android bringup&lt;/A&gt; &lt;/P&gt;&lt;P&gt;You can refer it. I have a hardware with modified boot fuses. Meanwhile, I will test in that hardware and will get back to you if I get any improvements. Hope someone from Freescale helps us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Vijai Kumar K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 12:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423635#M63979</guid>
      <dc:creator>vijaikumar</dc:creator>
      <dc:date>2015-05-26T12:56:18Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423636#M63980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; For Your 2-channel LPDDR2 configuration :&lt;BR /&gt;CS0 (channel 0) is responsible for the following address range of 512 MB : 0x1000_0000 - (0x3000_0000 - 1) &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;CS1 (channel 1) is responsible for the following address range of 512 MB : 0x8000_0000 - (0xA000_0000 - 1) &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 06:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423636#M63980</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-05-28T06:13:28Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423637#M63981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;YESSSSS, I DID IT!!!!!!! IT WORKS!!!!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is how I solved my problem:&lt;BR /&gt;1. I had to activate the GPIOs to override the Fuses on 0x450 by setting BOOT_MODE to '01' (not really nessesary but helpful to play with fuses).&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Note to me: I think BOOT_MODE '10' is better for my purposes -&amp;gt; test it later.&lt;/P&gt;&lt;P&gt;2. Set "DDR Memory Map default config" in BOOT_CFG3 to '10' with the now active GPIOs. This activates interleaving mode for LPDDR2 to achieve a continous memory.&lt;/P&gt;&lt;P&gt;3. Change the Script-Aid:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The memory doesn't have two chip-selects. Although there are two CS-Pins, only one is active!&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Activate Interleaving mode&lt;/P&gt;&lt;P&gt;4. Change RAM-Size calculation in board specific C-File for U-Boot: The function "imx_ddr_size()" ignores two-channel-mode. So you have to set:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; gd-&amp;gt;ram_size = (imx_ddr_size()*2); //imx_ddr_size() ignores two channel mode. So double the size here! (!!!!!quick and dirty code!!!!!)&lt;/P&gt;&lt;P&gt;5. In device tree set the memory to a start-address of 0x10000000 (Base Address of MMDC0) and the range to 0x40000000 (1GiB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I remember, this was all I had to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps someone else, too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 14:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423637#M63981</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2015-05-28T14:23:58Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423638#M63982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks &lt;SPAN class="j-post-author"&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/people/steffendoster"&gt;steffendoster&lt;/A&gt;&lt;/STRONG&gt;&lt;/SPAN&gt; for coming back to the community and sharing your solution. I was also able to solve it. I used fixed 2x32 mapping instead of interleaving. :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2015 09:32:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423638#M63982</guid>
      <dc:creator>vijaikumar</dc:creator>
      <dc:date>2015-06-10T09:32:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problems configuring 2-Channel LPDDR2 on i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423639#M63983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, there seem to be another issue with this LPDDR2 configuration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to boot from SD1 for a very, very, very long time now. But It simply doesn't start from SD-Card.&lt;/P&gt;&lt;P&gt;Now I think I know a little bit more about the problem:&lt;BR /&gt;The Bootloader isn't written correctly into RAM. Perhaps the RAM-Initialization is buggy. But I did the RAM-Configuration with the script-aid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the 2 channel LPDDR2 in interleaving mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The symptoms:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;I can't start from SD-Card. (Also I can not start from eMMC)&lt;/LI&gt;&lt;LI&gt;After a long reasearch, I figured out, that the RAM isn't written correctly:&lt;BR /&gt;Every "odd" 4kB of Data in it are corrupt.&lt;BR /&gt;I added an example Memorydump with loaded U-boot Data. The upper one shows the Memory how it should be, the lower one shows the end of a "even" 4kB block which is OK, while the beginning of the following "odd" 4kB block is corrupt:&lt;BR /&gt;some of the data which had to be written to "the left" are written to "the right".&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And this seems to be the reason, why u-boot doesn't start.&lt;BR /&gt;As I see, the configuration written to MMDC seems to be correct. My configuration and initialzation is attached in myboard.cfg.&lt;/P&gt;&lt;P&gt;Also the same configuration started by JTAG does work and start u-boot.&lt;/P&gt;&lt;P&gt;Is there a Timing Issue with the "faster" start from SD? How can I slow down the execution of myboard.cfg? Or Can I veryfy the correct setting?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2015 14:45:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-configuring-2-Channel-LPDDR2-on-i-MX6Q/m-p/423639#M63983</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2015-06-15T14:45:36Z</dc:date>
    </item>
  </channel>
</rss>