<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Android LP kernel 3.14 PCIe doesn't work on SabreSD hardware</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-LP-kernel-3-14-PCIe-doesn-t-work-on-SabreSD-hardware/m-p/423413#M63948</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I hope the following helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/506056"&gt;PCIe host failed to come up on Sabre SD on kernel 3.14.28&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Oct 2015 07:58:48 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-10-06T07:58:48Z</dc:date>
    <item>
      <title>Android LP kernel 3.14 PCIe doesn't work on SabreSD hardware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-LP-kernel-3-14-PCIe-doesn-t-work-on-SabreSD-hardware/m-p/423412#M63947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using a i.MX6QD with Android LP (5.1.1_beta) with kernel version 3.14 and the PCIe interface doesn't work on the SabreSD hardware. In the kernel log we get the following information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: phy link never came up&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: Failed to bring link up!&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: failed to initialize host&lt;/P&gt;&lt;P&gt;imx6q-pcie: probe of 1ffc000.pcie failed with error -22&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I added these changes to the kernel configuration to enable the PCIe support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;+CONFIG_PCI=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCI_MSI=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCI_IMX6=y&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;+CONFIG_MIGHT_HAVE_PCI=y&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;+CONFIG_PCI_QUIRKS=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCI_DOMAINS=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCI_SYSCALL=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCIE_DW=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCIEPORTBUS=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCIEAER=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCIEASPM=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCIEASPM_PERFORMANCE=y&lt;/P&gt;&lt;P&gt;+CONFIG_PCIE_PME=y&lt;/P&gt;&lt;P&gt;+CONFIG_OF_PCI=y&lt;/P&gt;&lt;P&gt;+CONFIG_OF_PCI_IRQ=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is that a know issue or is their a patch that can be applied to the kernel to fix that problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has Freescale verified the PCIe interface with this kernel version? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Sep 2015 12:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-LP-kernel-3-14-PCIe-doesn-t-work-on-SabreSD-hardware/m-p/423412#M63947</guid>
      <dc:creator>MikeEngel</dc:creator>
      <dc:date>2015-09-30T12:11:21Z</dc:date>
    </item>
    <item>
      <title>Re: Android LP kernel 3.14 PCIe doesn't work on SabreSD hardware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-LP-kernel-3-14-PCIe-doesn-t-work-on-SabreSD-hardware/m-p/423413#M63948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I hope the following helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/506056"&gt;PCIe host failed to come up on Sabre SD on kernel 3.14.28&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Oct 2015 07:58:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-LP-kernel-3-14-PCIe-doesn-t-work-on-SabreSD-hardware/m-p/423413#M63948</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-06T07:58:48Z</dc:date>
    </item>
  </channel>
</rss>