<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Wayland GPU memory leak when opening and closing windows</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-GPU-memory-leak-when-opening-and-closing-windows/m-p/422936#M63858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are no available information about plans to release a patch for L3.10.53. So, the general recommendation could be using L3.14.28 to apply the currently available patch.&lt;/P&gt;&lt;P&gt;Unfortunately, not additional tests of the patch over L3.10.53 are available, so you could try, but considering the update changes from L3.10.53 to L3.14.28.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Nov 2015 21:52:24 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2015-11-25T21:52:24Z</dc:date>
    <item>
      <title>Wayland GPU memory leak when opening and closing windows</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-GPU-memory-leak-when-opening-and-closing-windows/m-p/422935#M63857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are seeing GPU memory being leaked (seen with gmem_info) when a Wayland client process opens and closes multiple windows.&amp;nbsp; We are running kernel 3.10.53 and GPU software 5.0.11.p4.4 on an i.MX6Q processor.&amp;nbsp; How can we resolve this problem?&amp;nbsp; I see the release notes for BSPs which include 5.0.11.p4.5 seem to indicate this problem is fixed there ("MGS-528 [#ccc] Wayland does not free window memory until the application exits").&amp;nbsp; Can we use 5.0.11.p4.5 with a 3.10.53 kernel to fix the memory leak, while maintaining stability?&amp;nbsp; And will there be a patch release of a 3.10.53 based BSP which includes updated GPU software?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Nov 2015 23:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wayland-GPU-memory-leak-when-opening-and-closing-windows/m-p/422935#M63857</guid>
      <dc:creator>stephenminutill</dc:creator>
      <dc:date>2015-11-18T23:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: Wayland GPU memory leak when opening and closing windows</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wayland-GPU-memory-leak-when-opening-and-closing-windows/m-p/422936#M63858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are no available information about plans to release a patch for L3.10.53. So, the general recommendation could be using L3.14.28 to apply the currently available patch.&lt;/P&gt;&lt;P&gt;Unfortunately, not additional tests of the patch over L3.10.53 are available, so you could try, but considering the update changes from L3.10.53 to L3.14.28.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Nov 2015 21:52:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wayland-GPU-memory-leak-when-opening-and-closing-windows/m-p/422936#M63858</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-11-25T21:52:24Z</dc:date>
    </item>
  </channel>
</rss>