<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Freescale Development Board - Getting Linux to Boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Freescale-Development-Board-Getting-Linux-to-Boot/m-p/422582#M63807</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kevin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first please check connections:&lt;/P&gt;&lt;P&gt;connect the UBS OTG port (J505, bottom) from the SABRE SD to the computer.&lt;/P&gt;&lt;P&gt;connect the USB to SERIAL port (J509, bottom) from the SABRE SD to the computer.&lt;/P&gt;&lt;P&gt;Most simple way to prepare SD image with dd command, this is described in&lt;/P&gt;&lt;P&gt;sect.4.3.2 "Copying the full SD card image&amp;nbsp; Linux Guide" attached Linux Guide and&lt;/P&gt;&lt;P&gt;Demo Images:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board Support Packages (27)&lt;/P&gt;&lt;P&gt;L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)&lt;/P&gt;&lt;P&gt;i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo&lt;/P&gt;&lt;P&gt;Files and Linux BSP Documentation&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below presentation gives short quidelines for starting to work with board&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://2012ftf.ccidnet.com/pdf/0066.pdf" rel="nofollow"&gt;http://2012ftf.ccidnet.com/pdf/0066.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Oct 2015 01:54:21 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-10-01T01:54:21Z</dc:date>
    <item>
      <title>Freescale Development Board - Getting Linux to Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freescale-Development-Board-Getting-Linux-to-Boot/m-p/422581#M63806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been successfully using the&amp;nbsp; Boundary Devices&amp;nbsp; Sabre Lite board &lt;A href="http://boundarydevices.com/product/sabre-lite-imx6-sbc/" style="text-decoration: underline;" title="http://boundarydevices.com/product/sabre-lite-imx6-sbc/"&gt;http://boundarydevices.com/product/sabre-lite-imx6-sbc/ &lt;/A&gt;&amp;nbsp; both with a prebuilt Trusty image (from BD) and also built and run&amp;nbsp; YOCTO builds with no issues (have set uboot to simply jump to the SD card directly to get it to boot).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have now been given a Freescale development board &lt;A href="http://cache.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT" title="http://cache.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT"&gt;SABRE for Smart Devices Reference Design|Freescale&lt;/A&gt; which comes with an &lt;STRONG&gt;Android&lt;/STRONG&gt; SDcard which boots fine.&lt;/P&gt;&lt;P&gt;However I don't seem to be able to get any yocto build to even attempt to boot and this card doesn't appear to enter MFG mode so I can use the OTG interface to update uboot.&lt;/P&gt;&lt;P&gt;The BD board had switches to jump to OTG access however the new card apparently should default to that if it can't boot from any other medium; it doesn't appear to..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone else tried using this development board wrt Linux and if so can I have some clues as to, maybe what MACHINE I should use in YOCTO and/or why the MFG interface doesn't appear to work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kev &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Sep 2015 10:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freescale-Development-Board-Getting-Linux-to-Boot/m-p/422581#M63806</guid>
      <dc:creator>kevcal</dc:creator>
      <dc:date>2015-09-30T10:02:23Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale Development Board - Getting Linux to Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freescale-Development-Board-Getting-Linux-to-Boot/m-p/422582#M63807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kevin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first please check connections:&lt;/P&gt;&lt;P&gt;connect the UBS OTG port (J505, bottom) from the SABRE SD to the computer.&lt;/P&gt;&lt;P&gt;connect the USB to SERIAL port (J509, bottom) from the SABRE SD to the computer.&lt;/P&gt;&lt;P&gt;Most simple way to prepare SD image with dd command, this is described in&lt;/P&gt;&lt;P&gt;sect.4.3.2 "Copying the full SD card image&amp;nbsp; Linux Guide" attached Linux Guide and&lt;/P&gt;&lt;P&gt;Demo Images:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board Support Packages (27)&lt;/P&gt;&lt;P&gt;L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)&lt;/P&gt;&lt;P&gt;i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo&lt;/P&gt;&lt;P&gt;Files and Linux BSP Documentation&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below presentation gives short quidelines for starting to work with board&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://2012ftf.ccidnet.com/pdf/0066.pdf" rel="nofollow"&gt;http://2012ftf.ccidnet.com/pdf/0066.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Oct 2015 01:54:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freescale-Development-Board-Getting-Linux-to-Boot/m-p/422582#M63807</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-01T01:54:21Z</dc:date>
    </item>
  </channel>
</rss>