<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Android mm or mmm command in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-mm-or-mmm-command/m-p/422256#M63718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am new to Android. I have the entire source code of Android for the imx-6 platform. I would like to build the wpa_supplicant folder present under external folder. Everytime I make a change, instead of building the entire source, I would like to build only the wpa_supplicant folder. I have read that using the 'mm' command I can do it. However, i am not sure where to find the 'mm' command. For when I type #mm external/wpa_supplicant_8, I get the following error message displayed:&lt;/P&gt;&lt;P&gt;The program 'mm' can be found in the following packages: * mountmanager * multimail Try: apt-get install &lt;/P&gt;&lt;P&gt;I am not sure if I need to do an apt-get install or the binary is present somewhere I else. Can someone help me with this? Also, how do I compile only a single application present in external folder? Please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2015 07:25:21 GMT</pubDate>
    <dc:creator>Silwerstar</dc:creator>
    <dc:date>2015-05-12T07:25:21Z</dc:date>
    <item>
      <title>Android mm or mmm command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-mm-or-mmm-command/m-p/422256#M63718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am new to Android. I have the entire source code of Android for the imx-6 platform. I would like to build the wpa_supplicant folder present under external folder. Everytime I make a change, instead of building the entire source, I would like to build only the wpa_supplicant folder. I have read that using the 'mm' command I can do it. However, i am not sure where to find the 'mm' command. For when I type #mm external/wpa_supplicant_8, I get the following error message displayed:&lt;/P&gt;&lt;P&gt;The program 'mm' can be found in the following packages: * mountmanager * multimail Try: apt-get install &lt;/P&gt;&lt;P&gt;I am not sure if I need to do an apt-get install or the binary is present somewhere I else. Can someone help me with this? Also, how do I compile only a single application present in external folder? Please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 07:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-mm-or-mmm-command/m-p/422256#M63718</guid>
      <dc:creator>Silwerstar</dc:creator>
      <dc:date>2015-05-12T07:25:21Z</dc:date>
    </item>
    <item>
      <title>Re: Android mm or mmm command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-mm-or-mmm-command/m-p/422257#M63719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;STRONG style="font-size: 12.6000003814697px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;A href="https://community.nxp.com/people/Silwerstar"&gt;Silwerstar&lt;/A&gt;&lt;/STRONG&gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you encounter below problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The program 'mm' is currently not installed. You can install it by typing:&lt;/P&gt;&lt;P&gt;apt-get install multimail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need return your android root content.&lt;/P&gt;&lt;P&gt;source ./build/envsetup.sh&lt;/P&gt;&lt;P&gt;lunch (select your platform)&lt;/P&gt;&lt;P&gt;enter external/wpa_supplicant_8&lt;/P&gt;&lt;P&gt;execute 'mm'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 10:56:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-mm-or-mmm-command/m-p/422257#M63719</guid>
      <dc:creator>sanshanzhang</dc:creator>
      <dc:date>2015-05-12T10:56:19Z</dc:date>
    </item>
  </channel>
</rss>