<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How do I make imx6qsabresd into a DHCP server</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421779#M63613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Added the following to my eth0 interface:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; post-up /etc/init.d/dhcp-server start&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pre-down /etc/init.d/dhcp-server stop&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which fixes the automatic start/stop of the dhcp server.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Sep 2015 16:32:26 GMT</pubDate>
    <dc:creator>tfarnham</dc:creator>
    <dc:date>2015-09-17T16:32:26Z</dc:date>
    <item>
      <title>How do I make imx6qsabresd into a DHCP server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421775#M63609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having difficulty getting the sabre board to be a DHCP server for my network.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Within my own layer using the Yocto framework:&lt;/P&gt;&lt;P&gt;I have created a dhcp_%.bbappend &lt;/P&gt;&lt;P&gt;I have my own dhcpd.conf&lt;/P&gt;&lt;P&gt;I have my own default-server file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have validated that the created image does in fact include my versions of these files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I boot the image, I see the message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting DHCP server: No state is present for card imxhdmisoc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I must be missing something, or have the files configured incorrectly.&amp;nbsp; I am hoping someone has the proper setup steps for configuration, or possibly knows how I might go about troubleshooting the startup issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Terry Farnham&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 20:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421775#M63609</guid>
      <dc:creator>tfarnham</dc:creator>
      <dc:date>2015-09-02T20:56:21Z</dc:date>
    </item>
    <item>
      <title>Re: How do I make imx6qsabresd into a DHCP server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421776#M63610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually "No state is present for card" is not a error message. It is just a minor warning.&lt;/P&gt;&lt;P&gt;So please check if DHCP server is up and repliing the requests.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 14:27:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421776#M63610</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2015-09-03T14:27:53Z</dc:date>
    </item>
    <item>
      <title>Re: How do I make imx6qsabresd into a DHCP server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421777#M63611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I agree, the warning that appears seems to be unrelated as well.&amp;nbsp; I have been able to verify that I can successfully run the dhcpd daemon.&amp;nbsp; I do, however, have something incorrectly configured.&amp;nbsp; I'm guessing my dhcpd.conf file has something wrong.&amp;nbsp; My windows box issues the error upon dhcp renewal:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"An error occurred while renewing interface Ethernet : The parameter is incorrect."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the adapters are seeing the "foobar.com" DNS suffix&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my dhcpd.conf - maybe someone with better understanding can help me locate the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---------------------&lt;/P&gt;&lt;P&gt;default-lease-time 600;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # 10 minutes&lt;/P&gt;&lt;P&gt;max-lease-time 7200;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # 2&amp;nbsp; hours&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;option domain-name "foobar.com";&lt;/P&gt;&lt;P&gt;option domain-name-servers 10.0.0.1, 10.0.0.2;&lt;/P&gt;&lt;P&gt;option broadcast-address 10.0.0.255;&lt;/P&gt;&lt;P&gt;option routers 0.0.0.254;&lt;/P&gt;&lt;P&gt;option subnet-mask 255.255.255.0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;subnet 10.0.0.0 netmask 255.255.255.0&lt;/P&gt;&lt;P&gt; {&lt;/P&gt;&lt;P&gt;&amp;nbsp; range 10.0.0.10 10.0.0.20;&lt;/P&gt;&lt;P&gt;&amp;nbsp; range 10.0.0.100 10.0.0.200;&lt;/P&gt;&lt;P&gt; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 14:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421777#M63611</guid>
      <dc:creator>tfarnham</dc:creator>
      <dc:date>2015-09-04T14:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: How do I make imx6qsabresd into a DHCP server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421778#M63612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out my typo shortly after I posted:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;option routers 10.0.0.254;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I am still having difficulty getting the dhcp-server to actually startup properly at boot time.&amp;nbsp; I always seem to have to manually start it after boot up and login.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 15:14:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421778#M63612</guid>
      <dc:creator>tfarnham</dc:creator>
      <dc:date>2015-09-04T15:14:53Z</dc:date>
    </item>
    <item>
      <title>Re: How do I make imx6qsabresd into a DHCP server</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421779#M63613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Added the following to my eth0 interface:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; post-up /etc/init.d/dhcp-server start&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pre-down /etc/init.d/dhcp-server stop&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which fixes the automatic start/stop of the dhcp server.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 16:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-make-imx6qsabresd-into-a-DHCP-server/m-p/421779#M63613</guid>
      <dc:creator>tfarnham</dc:creator>
      <dc:date>2015-09-17T16:32:26Z</dc:date>
    </item>
  </channel>
</rss>