<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SABRE AI edige connector</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SABRE-AI-edige-connector/m-p/421158#M63504</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Takashi Matsuzawa,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a thread (link below) in which they mention how they used a Speedtech B35P101-01123-H connector so that would be the safest bet. Although I understand that this part number may not be easily available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/321210"&gt;Evalboard with i.mx6 and ETM/PTM connector&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Speedtech has a MXM 3.0 form-factor which should be the same as the EDM, which is the used on the Wandboard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Sep 2015 15:45:20 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2015-09-08T15:45:20Z</dc:date>
    <item>
      <title>SABRE AI edige connector</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SABRE-AI-edige-connector/m-p/421156#M63502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;Is anyone aware of easy solution to break out signals available on ESABRE AI board's edge connector (281 pins) so that I can try something.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The below post says there is a debug line breakout board for this.&lt;/P&gt;&lt;P&gt;I want to do similar, but with different line signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="392960" data-objecttype="2" href="https://community.freescale.com/message/392960#392960"&gt;https://community.freescale.com/message/392960&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The schematics says the socker prt # is follows, but it seems it is not easy to get at DYI shops.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPEEDTECH CORP&lt;/P&gt;&lt;P&gt;B35P101-01123-H&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's 0.5mm pitch, and maybe it could not be exactly be this part #, but currently have no idea of what easy-to-get connector kit is compatible with it.&lt;/P&gt;&lt;P&gt;Or, freescale has something (part kit) that can be used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know SABRE AI base board has socket for it, but I try to use SABRE AI CPU board standalone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 01:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SABRE-AI-edige-connector/m-p/421156#M63502</guid>
      <dc:creator>tmatsuzawa</dc:creator>
      <dc:date>2015-09-03T01:25:48Z</dc:date>
    </item>
    <item>
      <title>Re: SABRE AI edige connector</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SABRE-AI-edige-connector/m-p/421157#M63503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, after some research, I believe it is MXM 3.0 specification, and Wandboard's EDMCONNECTORKIT could be one option.&lt;/P&gt;&lt;P&gt;Any other experiences?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 11:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SABRE-AI-edige-connector/m-p/421157#M63503</guid>
      <dc:creator>tmatsuzawa</dc:creator>
      <dc:date>2015-09-04T11:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: SABRE AI edige connector</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SABRE-AI-edige-connector/m-p/421158#M63504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Takashi Matsuzawa,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a thread (link below) in which they mention how they used a Speedtech B35P101-01123-H connector so that would be the safest bet. Although I understand that this part number may not be easily available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/321210"&gt;Evalboard with i.mx6 and ETM/PTM connector&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Speedtech has a MXM 3.0 form-factor which should be the same as the EDM, which is the used on the Wandboard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 15:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SABRE-AI-edige-connector/m-p/421158#M63504</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-09-08T15:45:20Z</dc:date>
    </item>
  </channel>
</rss>