<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: &amp;quot;ROM Write failed&amp;quot; using DDR stress test 1.0.3 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/quot-ROM-Write-failed-quot-using-DDR-stress-test-1-0-3/m-p/421150#M63501</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;Indeed I was facing an issue with the OS, using VirtualBox and we should NEVER use it for this purpose. :smileyhappy:&lt;/P&gt;&lt;P&gt;Use a regular windows XP or later see.&lt;/P&gt;&lt;P&gt;Could be nice to have the same tool on Linux OS. :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Sep 2015 09:10:01 GMT</pubDate>
    <dc:creator>dabrain</dc:creator>
    <dc:date>2015-09-30T09:10:01Z</dc:date>
    <item>
      <title>"ROM Write failed" using DDR stress test 1.0.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-ROM-Write-failed-quot-using-DDR-stress-test-1-0-3/m-p/421148#M63499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently trying to bring up a board based on imx sabresd quad. I have been changing the DDR3 reference to 4 memory alliance AS4C256M16D3L chips.&lt;/P&gt;&lt;P&gt;When we are trying to use the DDR stress test tool over USB OTG, i'm getting an error "ROM write failed" with a random register after IOMUXC_SW_PAD_CTL_GRP_DDRMODE_CTL.&lt;/P&gt;&lt;P&gt;In this case, the board resets.&lt;/P&gt;&lt;P&gt;Could it be related to a bad software configuration or an hardware issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Sep 2015 16:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-ROM-Write-failed-quot-using-DDR-stress-test-1-0-3/m-p/421148#M63499</guid>
      <dc:creator>dabrain</dc:creator>
      <dc:date>2015-09-29T16:15:29Z</dc:date>
    </item>
    <item>
      <title>Re: "ROM Write failed" using DDR stress test 1.0.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-ROM-Write-failed-quot-using-DDR-stress-test-1-0-3/m-p/421149#M63500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cerveau&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;more likely this error is hardware, caused by usb malfunction,&lt;/P&gt;&lt;P&gt;so ROM fails to execute SDP WRITE REGISTER command.&lt;/P&gt;&lt;P&gt;One can try it with baremetal SDK usb test&lt;/P&gt;&lt;P&gt;"MX6_PLATFORM_SDK "&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="94139" data-objecttype="102" href="https://community.freescale.com/docs/DOC-94139"&gt;https://community.freescale.com/docs/DOC-94139&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also DDR stress can be run with jtag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Sep 2015 01:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-ROM-Write-failed-quot-using-DDR-stress-test-1-0-3/m-p/421149#M63500</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-30T01:56:33Z</dc:date>
    </item>
    <item>
      <title>Re: "ROM Write failed" using DDR stress test 1.0.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-ROM-Write-failed-quot-using-DDR-stress-test-1-0-3/m-p/421150#M63501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;Indeed I was facing an issue with the OS, using VirtualBox and we should NEVER use it for this purpose. :smileyhappy:&lt;/P&gt;&lt;P&gt;Use a regular windows XP or later see.&lt;/P&gt;&lt;P&gt;Could be nice to have the same tool on Linux OS. :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Sep 2015 09:10:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-ROM-Write-failed-quot-using-DDR-stress-test-1-0-3/m-p/421150#M63501</guid>
      <dc:creator>dabrain</dc:creator>
      <dc:date>2015-09-30T09:10:01Z</dc:date>
    </item>
  </channel>
</rss>