<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックno ppp on imx6 linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/no-ppp-on-imx6-linux/m-p/420213#M63374</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used fsl-arm-yocto-bsp, but after I build, no pppd in linux file system.&lt;/P&gt;&lt;P&gt;How can I build bsp with ppp inside.&lt;/P&gt;&lt;P&gt;ths&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Oct 2015 03:52:56 GMT</pubDate>
    <dc:creator>tonyzhou300</dc:creator>
    <dc:date>2015-10-22T03:52:56Z</dc:date>
    <item>
      <title>no ppp on imx6 linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/no-ppp-on-imx6-linux/m-p/420213#M63374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used fsl-arm-yocto-bsp, but after I build, no pppd in linux file system.&lt;/P&gt;&lt;P&gt;How can I build bsp with ppp inside.&lt;/P&gt;&lt;P&gt;ths&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2015 03:52:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/no-ppp-on-imx6-linux/m-p/420213#M63374</guid>
      <dc:creator>tonyzhou300</dc:creator>
      <dc:date>2015-10-22T03:52:56Z</dc:date>
    </item>
    <item>
      <title>Re: no ppp on imx6 linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/no-ppp-on-imx6-linux/m-p/420214#M63375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please add this command into conf/local.conf file inside your build directory:&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append = " ppp"&lt;/P&gt;&lt;P&gt;It should help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 05:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/no-ppp-on-imx6-linux/m-p/420214#M63375</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2015-11-03T05:41:28Z</dc:date>
    </item>
  </channel>
</rss>