<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックVideo playback issues</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Video-playback-issues/m-p/420041#M63323</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if anyone can help with a couple of video playback issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My setup is a core-image-sato build with gstreamer and chromium using the "Fido" branch of the fsl-community-bsp and I am playing a H.264 video file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Using the media player playback is good but if I put the display in to portrait mode using "xrandr" playback of the same video file is not good. CPU usage for gtk-play goes from 12% to 40%. Does anyone know if there are issues with hardware acceleration in portrait mode or a way to fix this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I've built chromium but I can't play any H.264 files at all. Does anyone know if chromium can play these files or how I go about getting them to play.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ian &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Oct 2015 08:59:33 GMT</pubDate>
    <dc:creator>IanCraig</dc:creator>
    <dc:date>2015-10-22T08:59:33Z</dc:date>
    <item>
      <title>Video playback issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-playback-issues/m-p/420041#M63323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if anyone can help with a couple of video playback issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My setup is a core-image-sato build with gstreamer and chromium using the "Fido" branch of the fsl-community-bsp and I am playing a H.264 video file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Using the media player playback is good but if I put the display in to portrait mode using "xrandr" playback of the same video file is not good. CPU usage for gtk-play goes from 12% to 40%. Does anyone know if there are issues with hardware acceleration in portrait mode or a way to fix this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I've built chromium but I can't play any H.264 files at all. Does anyone know if chromium can play these files or how I go about getting them to play.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ian &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2015 08:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-playback-issues/m-p/420041#M63323</guid>
      <dc:creator>IanCraig</dc:creator>
      <dc:date>2015-10-22T08:59:33Z</dc:date>
    </item>
    <item>
      <title>Re: Video playback issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-playback-issues/m-p/420042#M63324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Current xrand is supported however there are some features that are not accelerated by GPU, and this is marked as a bug. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="351854" data-objecttype="1" href="https://community.nxp.com/thread/351854"&gt;Reduced graphic performance with rotated screen (imx6, sabresd)&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Nov 2015 17:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-playback-issues/m-p/420042#M63324</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2015-11-10T17:13:10Z</dc:date>
    </item>
  </channel>
</rss>