<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 gstreamer camera source IPU/GPU rotate method?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/gstreamer-camera-source-IPU-GPU-rotate-method/m-p/418981#M63145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am trying to use the ov5640 camera with imx6qsabresd yocto project,&lt;/P&gt;&lt;P&gt;and I can use the following gstreamer command to show the preview from ov5640 to LCD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;gst-launch-1.0 imxv4l2src device=/dev/video1 ! 'video/x-raw, capture-mode=1, format=(string)NV12, width=640, height=480, framerate=(fraction)30/1' ! imxv4l2sink&lt;/P&gt;&lt;P&gt;I want to rotate the preview,&lt;/P&gt;&lt;P&gt;and I have tried the ! videoflip method=clockwise !&lt;/P&gt;&lt;P&gt;but it seems like a software method and it is too slow(very low fps).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any IPU/GPU or other HW method which can do the gstreamer rotate in high FPS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you and best regard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Sep 2015 08:06:51 GMT</pubDate>
    <dc:creator>stevesu</dc:creator>
    <dc:date>2015-09-02T08:06:51Z</dc:date>
    <item>
      <title>gstreamer camera source IPU/GPU rotate method?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gstreamer-camera-source-IPU-GPU-rotate-method/m-p/418981#M63145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am trying to use the ov5640 camera with imx6qsabresd yocto project,&lt;/P&gt;&lt;P&gt;and I can use the following gstreamer command to show the preview from ov5640 to LCD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;gst-launch-1.0 imxv4l2src device=/dev/video1 ! 'video/x-raw, capture-mode=1, format=(string)NV12, width=640, height=480, framerate=(fraction)30/1' ! imxv4l2sink&lt;/P&gt;&lt;P&gt;I want to rotate the preview,&lt;/P&gt;&lt;P&gt;and I have tried the ! videoflip method=clockwise !&lt;/P&gt;&lt;P&gt;but it seems like a software method and it is too slow(very low fps).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any IPU/GPU or other HW method which can do the gstreamer rotate in high FPS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you and best regard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 08:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gstreamer-camera-source-IPU-GPU-rotate-method/m-p/418981#M63145</guid>
      <dc:creator>stevesu</dc:creator>
      <dc:date>2015-09-02T08:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: gstreamer camera source IPU/GPU rotate method?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gstreamer-camera-source-IPU-GPU-rotate-method/m-p/418982#M63146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steve&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at attached Linux Guide from Linux 3.14.28&lt;/P&gt;&lt;P&gt;sect.7.5.3 Video conversion, some useful gstreamer commands below&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/Freescale/gstreamer-imx" title="https://github.com/Freescale/gstreamer-imx"&gt;Freescale/gstreamer-imx · GitHub&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 01:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gstreamer-camera-source-IPU-GPU-rotate-method/m-p/418982#M63146</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-03T01:41:23Z</dc:date>
    </item>
  </channel>
</rss>