<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How can I set IOMUX Pin for using gpio?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-set-IOMUX-Pin-for-using-gpio/m-p/418795#M63109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please refer to Chapter 2 (Configuring the IOMUX Controller)&lt;BR /&gt;of "i.MX_6_BSP_Porting_Guide.pdf". Also, "for details, see:&lt;/P&gt;&lt;P&gt;Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt&lt;/P&gt;&lt;P&gt;Documentation/devicetree/bindings/pinctrl/fsl,imx6*-pinctrl.txt"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jun 2015 02:18:15 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-06-23T02:18:15Z</dc:date>
    <item>
      <title>How can I set IOMUX Pin for using gpio?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-set-IOMUX-Pin-for-using-gpio/m-p/418794#M63108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I set IOMUX Pin for using gpio(Pull up)?&lt;/P&gt;&lt;P&gt;Actually I try to change dts like below but it's not work.&lt;/P&gt;&lt;P&gt;I want to use checking MDM status pin of GPIO5_28.&lt;/P&gt;&lt;P&gt;So I add Pin control as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Mux Setting Pin : CSI0_DAT10&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;arch/arm/boot/dts/imx6q-pinfunc.h:803:#define MX6QDL_PAD_CSI0_DAT10__GPIO5_IO28&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x280 0x650 0x000 0x5 0x0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Control Setting Pin &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;--- a/arch/arm/boot/dts/imx6qdl.dtsi&lt;/P&gt;&lt;P&gt;+++ b/arch/arm/boot/dts/imx6qdl.dtsi&lt;/P&gt;&lt;P&gt;@@ -1602,6 +1602,12 @@&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6QDL_PAD_RGMII_RXC__USB_H3_STROBE 0x40017030&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl_usbh3_3: usbh3grp-3 {&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,pins = &amp;lt;&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;STRONG&gt;MX6QDL_PAD_CSI0_DAT10__GPIO5_IO28&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x1b0b1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;gt;;&lt;/P&gt;&lt;P&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you share What i do to use it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 12:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-set-IOMUX-Pin-for-using-gpio/m-p/418794#M63108</guid>
      <dc:creator>chesterkang</dc:creator>
      <dc:date>2015-06-22T12:20:12Z</dc:date>
    </item>
    <item>
      <title>Re: How can I set IOMUX Pin for using gpio?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-set-IOMUX-Pin-for-using-gpio/m-p/418795#M63109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please refer to Chapter 2 (Configuring the IOMUX Controller)&lt;BR /&gt;of "i.MX_6_BSP_Porting_Guide.pdf". Also, "for details, see:&lt;/P&gt;&lt;P&gt;Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt&lt;/P&gt;&lt;P&gt;Documentation/devicetree/bindings/pinctrl/fsl,imx6*-pinctrl.txt"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2015 02:18:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-set-IOMUX-Pin-for-using-gpio/m-p/418795#M63109</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-06-23T02:18:15Z</dc:date>
    </item>
  </channel>
</rss>