<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Can LVDS share same clock as IPU_DIx post PODF?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-LVDS-share-same-clock-as-IPU-DIx-post-PODF/m-p/418544#M63076</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no, there is no path to feed output DI clock into LVDS.&lt;/P&gt;&lt;P&gt;Only available options are given in CCM Chapter of Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Nov 2015 01:37:33 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-11-18T01:37:33Z</dc:date>
    <item>
      <title>Can LVDS share same clock as IPU_DIx post PODF?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-LVDS-share-same-clock-as-IPU-DIx-post-PODF/m-p/418543#M63075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I understand it the LVDS channels can use one of 5 clocks,&lt;/P&gt;&lt;P&gt;000 pll5 clock&lt;/P&gt;&lt;P&gt;001 pll2 352M PFD&lt;/P&gt;&lt;P&gt;010 pll2 396M PFD&lt;/P&gt;&lt;P&gt;011 MMDC_CH1 clock&lt;/P&gt;&lt;P&gt;100 pll3_sw_clk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and it can also have a post 3.5/7 divider on that clock. &lt;/P&gt;&lt;P&gt;We use pll5 as our IPU DI clock parent.&amp;nbsp; We further use CHSCCDR and CSCDR2 to divide the clock some more to drive the DI. &lt;/P&gt;&lt;P&gt;Is there a way to reuse that same clock the DI is using as the LVDS clock?&amp;nbsp;&amp;nbsp; I can't seem to see that anywhere in the reference manual.&amp;nbsp; For example the parallel RGB is fine in this case because it uses the output DI clock.&amp;nbsp;&amp;nbsp; I would have thought that there would be a path to feed that output DI clock into LVDS. &lt;/P&gt;&lt;P&gt;Is this possible? Is there something I am missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Nov 2015 15:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-LVDS-share-same-clock-as-IPU-DIx-post-PODF/m-p/418543#M63075</guid>
      <dc:creator>tommalnar</dc:creator>
      <dc:date>2015-11-17T15:21:47Z</dc:date>
    </item>
    <item>
      <title>Re: Can LVDS share same clock as IPU_DIx post PODF?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-LVDS-share-same-clock-as-IPU-DIx-post-PODF/m-p/418544#M63076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no, there is no path to feed output DI clock into LVDS.&lt;/P&gt;&lt;P&gt;Only available options are given in CCM Chapter of Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Nov 2015 01:37:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-LVDS-share-same-clock-as-IPU-DIx-post-PODF/m-p/418544#M63076</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-18T01:37:33Z</dc:date>
    </item>
  </channel>
</rss>