<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: mfgtool2 eMMC flashing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417280#M62740</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ritesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try&amp;nbsp; demo images (place them in MFG Tools folder)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.0.35_4.1.0_DEMO_IMAGE_BSP&lt;/A&gt;&amp;nbsp; : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,&lt;/P&gt;&lt;P&gt;i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Entering to Serial Downloader mode is not supported directly, say for&amp;nbsp; the&lt;/P&gt;&lt;P&gt;i.MX6 SDP / SDB designs. According to section 4.1 (How to Enter Serial Download Mode&lt;/P&gt;&lt;P&gt;for MFGTool)of "i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf" :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; "No dedicated boot dips are reserved for serial download mode on i.MX 6 SABRE-SD&lt;/P&gt;&lt;P&gt;boards. Therefore, a tricky method is used to enter serial download mode. For example,&lt;/P&gt;&lt;P&gt;set boot mode as SD3 boot (SW6 dip 2, 7 on others are off). Do not insert SD card into&lt;/P&gt;&lt;P&gt;SD3 slot, and power on the board. After "HID- Compliant device" is detected, it means&lt;/P&gt;&lt;P&gt;that the board has entered serial download mode. Insert the SD card into SD3 slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can also flash SD card on Host computer, as describes&lt;/P&gt;&lt;P&gt;Chapter 8 Using a Linux Host to Set Up an SD/MMC Card attached Linux Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 21 Jun 2015 17:06:43 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-06-21T17:06:43Z</dc:date>
    <item>
      <title>mfgtool2 eMMC flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417278#M62738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using imx6qsabresd board. And using yocto v3.14.28.1.0.0.&lt;/P&gt;&lt;P&gt;I want to flash image created using bitbake into eMMC of the board.&lt;/P&gt;&lt;P&gt;I refered iMX6 linux user guide. But i am unable to understand.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please find default cfg.ini and ucl2.xml files.&lt;/P&gt;&lt;P&gt;And if i change the LIST&amp;nbsp; name=eMMC in cfg.ini and try to open mfgtool2.exe i got error "Iitialize operation failed error code-4".&lt;/P&gt;&lt;P&gt;so what's the problem? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So&lt;/P&gt;&lt;P&gt;1. What's the correct settings for cfg.ini &amp;amp; ucl2.xml for eMMC&lt;/P&gt;&lt;P&gt;2. how to run mfgtool2?&lt;/P&gt;&lt;P&gt;3. what should be the Switch setting of SW6 for flashing?&lt;/P&gt;&lt;P&gt;4. how to add my .ext3 image file?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335830"&gt;ucl2.xml.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335830"&gt;cfg.ini.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Jun 2015 12:54:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417278#M62738</guid>
      <dc:creator>riteshpanchal</dc:creator>
      <dc:date>2015-06-20T12:54:27Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool2 eMMC flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417279#M62739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok. My mistake. I am using the wrong mfgtool. &lt;/P&gt;&lt;P&gt;I found the new "Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER" and i just change the list name=SabreSD-eMMC&lt;/P&gt;&lt;P&gt;And make SW6 setting = 00001100 (low to high). &lt;/P&gt;&lt;P&gt;And press the start button. And all process done successfully.&lt;/P&gt;&lt;P&gt;But then change SW6 to 11010110 (low to high). But nothing appears on screen or UART terminal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to flash my .ext3 image using mfgtool?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Jun 2015 13:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417279#M62739</guid>
      <dc:creator>riteshpanchal</dc:creator>
      <dc:date>2015-06-20T13:35:40Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool2 eMMC flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417280#M62740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ritesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try&amp;nbsp; demo images (place them in MFG Tools folder)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.0.35_4.1.0_DEMO_IMAGE_BSP&lt;/A&gt;&amp;nbsp; : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,&lt;/P&gt;&lt;P&gt;i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Entering to Serial Downloader mode is not supported directly, say for&amp;nbsp; the&lt;/P&gt;&lt;P&gt;i.MX6 SDP / SDB designs. According to section 4.1 (How to Enter Serial Download Mode&lt;/P&gt;&lt;P&gt;for MFGTool)of "i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf" :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; "No dedicated boot dips are reserved for serial download mode on i.MX 6 SABRE-SD&lt;/P&gt;&lt;P&gt;boards. Therefore, a tricky method is used to enter serial download mode. For example,&lt;/P&gt;&lt;P&gt;set boot mode as SD3 boot (SW6 dip 2, 7 on others are off). Do not insert SD card into&lt;/P&gt;&lt;P&gt;SD3 slot, and power on the board. After "HID- Compliant device" is detected, it means&lt;/P&gt;&lt;P&gt;that the board has entered serial download mode. Insert the SD card into SD3 slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can also flash SD card on Host computer, as describes&lt;/P&gt;&lt;P&gt;Chapter 8 Using a Linux Host to Set Up an SD/MMC Card attached Linux Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Jun 2015 17:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417280#M62740</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-21T17:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool2 eMMC flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417281#M62741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following changes i did.&lt;/P&gt;&lt;P&gt;1. &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;&lt;STRONG&gt;list name=SabreSD-eMMC&lt;/STRONG&gt; in &lt;STRONG&gt;cfg.ini&lt;/STRONG&gt; file&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;2. I deleted '&lt;STRONG&gt;rootfs.tar.bz2'&lt;/STRONG&gt; file in &lt;/SPAN&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;'Mfgtools-Rel-&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\files' folder and paste my&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt; "fsl-image-multimedia-full-imx6qsabresd-20150620054618.rootfs.tar.bz2" and renamed it to &lt;STRONG style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;rootfs.tar.bz2.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; line-height: 1.5;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;And than i changed all SW6 switches to off. press start button and completed the whole procedure.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;And after that modify SW6 for eMMC boot but nothing boot up&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;So i think i need to replace some more files in file folder.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;So can you list out which files need to replace? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 06:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417281#M62741</guid>
      <dc:creator>riteshpanchal</dc:creator>
      <dc:date>2015-06-22T06:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool2 eMMC flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417282#M62742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;are you able to boot from this board using other ways, for example SD ?&lt;/P&gt;&lt;P&gt;SD card can be flashed using Host computer, as describes&lt;/P&gt;&lt;P&gt;Chapter 8 Using a Linux Host to Set Up an SD/MMC Card attached Linux Guide&lt;/P&gt;&lt;P&gt;in previous answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 07:02:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417282#M62742</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-22T07:02:26Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool2 eMMC flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417283#M62743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If i flash my image using followinf linux command i can able to boot and run linux on board.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;$ sudo dd if=&amp;lt;image name&amp;gt;.sdcard of=/dev/sd&amp;lt;partition&amp;gt; bs=1M &amp;amp;&amp;amp; sync&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But now i want to flash this image to eMMC. So i am using mfgtool.&lt;/P&gt;&lt;P&gt;So am i need to add/replace any other file in file folder like .bin .dtb etc??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 07:12:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417283#M62743</guid>
      <dc:creator>riteshpanchal</dc:creator>
      <dc:date>2015-06-22T07:12:59Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool2 eMMC flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417284#M62744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After flashing using mfgtool i got u-boot interface after reset. But in Autoboot nothing boots up.&lt;/P&gt;&lt;P&gt;And in terminal i receiving continuously belowed message.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;## Warning: gatewayip needed but not set&lt;/P&gt;&lt;P&gt;FEC: Link is down 7949&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 08:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool2-eMMC-flashing/m-p/417284#M62744</guid>
      <dc:creator>riteshpanchal</dc:creator>
      <dc:date>2015-06-22T08:57:41Z</dc:date>
    </item>
  </channel>
</rss>