<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: getting frame data from /dev/video1 for processing and displaying, Linux on iMX6Q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/getting-frame-data-from-dev-video1-for-processing-and-displaying/m-p/417189#M62726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the mxc_vpu_test.out source code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for test, here is the command&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;modprobe ov5640_camera_mipi&lt;BR /&gt;modprobe ov5642_camera&lt;BR /&gt;modprobe mxc_v4l2_capture&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/unit_tests/mxc_vpu_test.out -E "-x 0 -o /enc.h264 -w 720 -h 480&amp;nbsp;&amp;nbsp; -c 5000 -f 2"&lt;/P&gt;&lt;P&gt; -x &amp;lt;input method&amp;gt; input mode V4L2 with video node&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 - /dev/video0, 1 - /dev/video1, and so on&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then you can play the enc.h264 with following command&lt;/P&gt;&lt;P&gt;/unit_tests/mxc_vpu_test.out&amp;nbsp; -D "-i /enc.h264 "&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Aug 2015 05:00:00 GMT</pubDate>
    <dc:creator>BiyongSUN</dc:creator>
    <dc:date>2015-08-06T05:00:00Z</dc:date>
    <item>
      <title>getting frame data from /dev/video1 for processing and displaying, Linux on iMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/getting-frame-data-from-dev-video1-for-processing-and-displaying/m-p/417187#M62724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to write a terminal app which init the camera and manipulate the input frame by frame on a pixel level before displaying to LCD or storing to disk.&lt;/P&gt;&lt;P&gt;Can anyone point me in the right direction on how to get started? I am very new to programming in Linux, any documentation or sample code would be very helpful.&lt;/P&gt;&lt;P&gt;I am currently running an unmodified fsl-image-qt5-x11-imx6qdlsolo image on the i.MX6Q Sabre-SD Platform board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 16:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/getting-frame-data-from-dev-video1-for-processing-and-displaying/m-p/417187#M62724</guid>
      <dc:creator>jingyizhang</dc:creator>
      <dc:date>2015-08-05T16:23:20Z</dc:date>
    </item>
    <item>
      <title>Re: getting frame data from /dev/video1 for processing and displaying, Linux on iMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/getting-frame-data-from-dev-video1-for-processing-and-displaying/m-p/417188#M62725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; General information how to use V4L2 API (with examples) may be found at &lt;BR /&gt; &lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://linuxtv.org/downloads/v4l-dvb-apis/" rel="nofollow"&gt;http://linuxtv.org/downloads/v4l-dvb-apis/&lt;/A&gt;&lt;BR /&gt; &lt;BR /&gt; Also, it makes sense to look at Chapter 9 [Video for Linux Two (V4L2) &lt;BR /&gt; Driver ] of “i.MX_6_Linux_Reference_Manual.pdf” ; in particular – section &lt;BR /&gt; 9.5.2 (Video4Linux API test).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product"&gt;https://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product&lt;/A&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;BR /&gt; You may to look to test sources on the host Linux :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;/fsl-release-bsp/tmp/work/-poky-linux-gnueabi/imx-test/&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Inside each test’s directory you will find the available documentation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 02:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/getting-frame-data-from-dev-video1-for-processing-and-displaying/m-p/417188#M62725</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-06T02:16:14Z</dc:date>
    </item>
    <item>
      <title>Re: getting frame data from /dev/video1 for processing and displaying, Linux on iMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/getting-frame-data-from-dev-video1-for-processing-and-displaying/m-p/417189#M62726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the mxc_vpu_test.out source code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for test, here is the command&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;modprobe ov5640_camera_mipi&lt;BR /&gt;modprobe ov5642_camera&lt;BR /&gt;modprobe mxc_v4l2_capture&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/unit_tests/mxc_vpu_test.out -E "-x 0 -o /enc.h264 -w 720 -h 480&amp;nbsp;&amp;nbsp; -c 5000 -f 2"&lt;/P&gt;&lt;P&gt; -x &amp;lt;input method&amp;gt; input mode V4L2 with video node&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 - /dev/video0, 1 - /dev/video1, and so on&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then you can play the enc.h264 with following command&lt;/P&gt;&lt;P&gt;/unit_tests/mxc_vpu_test.out&amp;nbsp; -D "-i /enc.h264 "&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 05:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/getting-frame-data-from-dev-video1-for-processing-and-displaying/m-p/417189#M62726</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2015-08-06T05:00:00Z</dc:date>
    </item>
  </channel>
</rss>