<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCIe, diagnosing and improving eye diagram in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416433#M62556</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;I have implemented a design that uses PCIe. It is somewhat different in that the PCIe interface is used as a chip-to-chip communication lane on a single PCB (e.g. no PCIe connector).&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;The root complex device is a Freescale i.MX6 Dual which is PCIe Gen 2 compliant and the device I am communicating with is a Marvell WiFi module that is a PCIe Gen 3 compliant device. It's a single lane interface running at 2.5Gbps.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;I've done some signal integrity measurements by soldering a high speed scope with proper differential probes right on the other side of the inline caps shown below. The total link/route length is about 2.5 inches. The i.MX6 is on a SOM while the WiFi module is on a PCB I designed. About half of the channel routing distance is on the SOM and the rest on the carrier board. The coupling caps are placed near the WiFi module which probably increasing the amount of reflections.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;&lt;IMG alt="enter image description here" class="jive-image" src="http://i.stack.imgur.com/VrZlE.png" /&gt;&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;For the clock the eye diagram looks quite good:&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;&lt;IMG alt="enter image description here" class="jive-image" src="http://i.stack.imgur.com/hI8xj.png" /&gt;&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;But the TX data not so much:&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;&lt;IMG alt="enter image description here" class="jive-image" src="http://i.stack.imgur.com/RFUfo.png" /&gt;&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;The WiFi chip has on-chip terminations so I don't believe I am supposed to need any additional terminations, but I could be wrong about that.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;We are in FULL SWING mode and set the register to the max value. We have played with the PCIe Gen 1 value and the above eye represents about the best we can find at 6'h7. It seems like each of the DEEMPH registers do the same thing and so the actual one that is selected may not matter.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;&lt;IMG alt="enter image description here" class="jive-image" src="http://i.stack.imgur.com/bZ4f6.png" /&gt;&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;I've checked that the layout follows proper routing rules and the PCB was constructed with the correct impedance. The coupling caps are 0402 in size. Obviously I have some jitter in the system but it also looks like I have a reflection or de-emphasis issue. I'm hoping someone could describe what they see wrong with my eye diagram and/or suggest some ways to fix it.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;NoteL We are not entering into compliance mode and just doing this testing on the standard link traffic. If we force entry into compliance mode via software the eye diagram actually gets worse but it also looks like it messes with a number of the other channel settings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jul 2015 22:11:35 GMT</pubDate>
    <dc:creator>georgekellerman</dc:creator>
    <dc:date>2015-07-15T22:11:35Z</dc:date>
    <item>
      <title>PCIe, diagnosing and improving eye diagram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416433#M62556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;I have implemented a design that uses PCIe. It is somewhat different in that the PCIe interface is used as a chip-to-chip communication lane on a single PCB (e.g. no PCIe connector).&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;The root complex device is a Freescale i.MX6 Dual which is PCIe Gen 2 compliant and the device I am communicating with is a Marvell WiFi module that is a PCIe Gen 3 compliant device. It's a single lane interface running at 2.5Gbps.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;I've done some signal integrity measurements by soldering a high speed scope with proper differential probes right on the other side of the inline caps shown below. The total link/route length is about 2.5 inches. The i.MX6 is on a SOM while the WiFi module is on a PCB I designed. About half of the channel routing distance is on the SOM and the rest on the carrier board. The coupling caps are placed near the WiFi module which probably increasing the amount of reflections.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;&lt;IMG alt="enter image description here" class="jive-image" src="http://i.stack.imgur.com/VrZlE.png" /&gt;&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;For the clock the eye diagram looks quite good:&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;&lt;IMG alt="enter image description here" class="jive-image" src="http://i.stack.imgur.com/hI8xj.png" /&gt;&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;But the TX data not so much:&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;&lt;IMG alt="enter image description here" class="jive-image" src="http://i.stack.imgur.com/RFUfo.png" /&gt;&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;The WiFi chip has on-chip terminations so I don't believe I am supposed to need any additional terminations, but I could be wrong about that.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;We are in FULL SWING mode and set the register to the max value. We have played with the PCIe Gen 1 value and the above eye represents about the best we can find at 6'h7. It seems like each of the DEEMPH registers do the same thing and so the actual one that is selected may not matter.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;&lt;IMG alt="enter image description here" class="jive-image" src="http://i.stack.imgur.com/bZ4f6.png" /&gt;&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;I've checked that the layout follows proper routing rules and the PCB was constructed with the correct impedance. The coupling caps are 0402 in size. Obviously I have some jitter in the system but it also looks like I have a reflection or de-emphasis issue. I'm hoping someone could describe what they see wrong with my eye diagram and/or suggest some ways to fix it.&lt;/P&gt;&lt;P style="margin-bottom: 1em; font-size: 15px; color: #333333; font-family: Georgia, 'Times New Roman', Times, serif; background-color: #fffef9;"&gt;NoteL We are not entering into compliance mode and just doing this testing on the standard link traffic. If we force entry into compliance mode via software the eye diagram actually gets worse but it also looks like it messes with a number of the other channel settings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 22:11:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416433#M62556</guid>
      <dc:creator>georgekellerman</dc:creator>
      <dc:date>2015-07-15T22:11:35Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe, diagnosing and improving eye diagram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416434#M62557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; HW Design Checking List for i.Mx6DQSDL Rev2.8 contains useful recommendations&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;about using (external) PCIe clock :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt; "Due to CLKx_P/N is LVDS port and don't match with PCIe reference clock specification.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;For PCIe Gen1 application, following low cost solution can be used(DC bias and AC&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;impedance should be considered).&amp;nbsp; Please refer to "HW Design Checking List for i.Mx6DQSDL&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Rev2.7.xlsx", sheet "Schematic", Ref12 for more info."&lt;BR /&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; "PCIe reference clock solution which provided by CLKx_N/P of i.MX6 chip can't pass PCIe&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Gen2 compliance test.&amp;nbsp; Recommend using external PCIe 2.0/3.0 clock generator with 2 HCSL&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;outputs solution. One clock channel connect to i.MX6 as a reference input, please click&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Ref14 ("HW Design Checking List for i.Mx6DQSDL Rev2.7.xlsx") for reference circuit.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Another clock channel should connect to PCIe connector, please contact generator vendor&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;for detailed design guide."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="93819" data-objecttype="102" href="https://community.freescale.com/docs/DOC-93819"&gt;https://community.freescale.com/docs/DOC-93819&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; The PCIe clock signal pair is not part of the PCIe PHY IP (assuming the CLK1N/P are used).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;They are configured via&amp;nbsp; PMU_MISC1n register.&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 05:11:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416434#M62557</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-07-21T05:11:45Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe, diagnosing and improving eye diagram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416435#M62558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response and the resource link. I have gone though it and unfortunately I do not think much of it can be applied to this particular issue. In my case the eye diagram for my clock is quite clean. I believe the recommendation in Ref12 could potentially clean up the clock even more but it wouldn't clean up the TX/RX eye diagram.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also as mentioned the i.MX6 is on a third-party SOM that I don't have control over the i.MX6 side of things.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do notice that 85ohm differential is recommended for the TX/RX signals. Do you know why this is since PCIe specifies 100ohm? I confirmed with the SOM vendor that they routed PCIe @ 100ohms so I think it would make it worse to change my board to 85 ohms since there would be an impedance mismatch.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 21:02:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416435#M62558</guid>
      <dc:creator>georgekellerman</dc:creator>
      <dc:date>2015-07-21T21:02:26Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe, diagnosing and improving eye diagram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416436#M62559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;1. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; Your clock solution may be used for the gen1, but for the gen2 external &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;external PCIe 2.0/3.0 clock generator with 2 HCSL outputs should be applied.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;2. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; It is good idea to be orinted on PCIe specifications regarding nominal impedance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Basically value of 85 Ohm is in specified range . I think the i.MX6 is able to work with &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;85 Ohm impedance, however more correct answer can be obtained using simulations &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;or real board tests.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;BR /&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;The latest PCIe rev.3.0 defines 85 Ohm impedance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Yuri.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-family: Verdana, sans-serif;"&gt;&lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 06:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416436#M62559</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-07-23T06:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe, diagnosing and improving eye diagram</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416437#M62560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/georgekellerman"&gt;georgekellerman&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My custom hardware is based on iMAX6Q processor and I need to check PCIE signal integrity using eye diagram. According to NXP manual they have recommend to use oscilloscope: Tektronix MSO72004C which is very expensive with its differential pair probes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What kind of oscilloscope did you use for above testings ? Any suggestion to observer the PCIE signal integrity ? Do you know any lab space around Asia or Europe which we can use for testings with charges ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards &amp;amp; Thanks,&lt;/P&gt;&lt;P&gt;Peter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Dec 2018 10:22:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-diagnosing-and-improving-eye-diagram/m-p/416437#M62560</guid>
      <dc:creator>peteramond</dc:creator>
      <dc:date>2018-12-13T10:22:26Z</dc:date>
    </item>
  </channel>
</rss>