<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6Q Linux and new clock in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Linux-and-new-clock/m-p/415391#M62404</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom audio board that requires its own clock based on the PLL4 clock with its own multiplier and divider. Is it necessary to add a new clock listed in /arch/arm/mach-imx/clk-imx6q.c or is it possible to add this information to the device tree? I know I can modify the registers directly in a driver but I am trying to determine the best practice based on the architecture that already exists.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Sep 2015 07:29:09 GMT</pubDate>
    <dc:creator>nwwinters</dc:creator>
    <dc:date>2015-09-01T07:29:09Z</dc:date>
    <item>
      <title>i.MX6Q Linux and new clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Linux-and-new-clock/m-p/415391#M62404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom audio board that requires its own clock based on the PLL4 clock with its own multiplier and divider. Is it necessary to add a new clock listed in /arch/arm/mach-imx/clk-imx6q.c or is it possible to add this information to the device tree? I know I can modify the registers directly in a driver but I am trying to determine the best practice based on the architecture that already exists.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 07:29:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Linux-and-new-clock/m-p/415391#M62404</guid>
      <dc:creator>nwwinters</dc:creator>
      <dc:date>2015-09-01T07:29:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q Linux and new clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Linux-and-new-clock/m-p/415392#M62405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Nick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if clock is not used in linux, one can program it in dcd header.&lt;/P&gt;&lt;P&gt;For usage in linux one can refer to documentation:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/torvalds/linux/blob/master/Documentation/devicetree/bindings/clock/imx6q-clock.txt" title="https://github.com/torvalds/linux/blob/master/Documentation/devicetree/bindings/clock/imx6q-clock.txt"&gt;linux/imx6q-clock.txt at master · torvalds/linux · GitHub&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 02:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-Linux-and-new-clock/m-p/415392#M62405</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-03T02:50:15Z</dc:date>
    </item>
  </channel>
</rss>