<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6 FCPBGA thermal interface pad in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCPBGA-thermal-interface-pad/m-p/414897#M62238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am designing a product that has an IMX6 processor in an FCPBGA package. The main PCB is mounted in an aluminum enclosure, which I would also like to use as a heatsink for the IMX6. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A thermal gap pad is placed between the enclosure and the IMX6 for optimal heat transfer. The pad is kept in place by the pressure of the case on the PCB. I have mechanical information about the pad (hardness, thickness, Young's Modulus), but I don't know how much pressure can be applied on the FCPBGA package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any information available from Freescale regarding about the maximum pressure that can be applied without damaging the package?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Nov 2015 13:38:42 GMT</pubDate>
    <dc:creator>sammypeiren</dc:creator>
    <dc:date>2015-11-16T13:38:42Z</dc:date>
    <item>
      <title>IMX6 FCPBGA thermal interface pad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCPBGA-thermal-interface-pad/m-p/414897#M62238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am designing a product that has an IMX6 processor in an FCPBGA package. The main PCB is mounted in an aluminum enclosure, which I would also like to use as a heatsink for the IMX6. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A thermal gap pad is placed between the enclosure and the IMX6 for optimal heat transfer. The pad is kept in place by the pressure of the case on the PCB. I have mechanical information about the pad (hardness, thickness, Young's Modulus), but I don't know how much pressure can be applied on the FCPBGA package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any information available from Freescale regarding about the maximum pressure that can be applied without damaging the package?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Nov 2015 13:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCPBGA-thermal-interface-pad/m-p/414897#M62238</guid>
      <dc:creator>sammypeiren</dc:creator>
      <dc:date>2015-11-16T13:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 FCPBGA thermal interface pad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCPBGA-thermal-interface-pad/m-p/414898#M62239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sammy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;maximum pressure is described on p.44 FCPBGA presentation &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/package_info/FC-PBGAPRES.pdf" rel="nofollow"&gt;http://cache.freescale.com/files/32bit/doc/package_info/FC-PBGAPRES.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Nov 2015 01:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCPBGA-thermal-interface-pad/m-p/414898#M62239</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-17T01:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 FCPBGA thermal interface pad</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCPBGA-thermal-interface-pad/m-p/414899#M62240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alright so anything below 45N should be acceptable? I assume PoP versions of the IMX6 are a bit more fragile, or can they handle the same pressure?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Nov 2015 12:17:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-FCPBGA-thermal-interface-pad/m-p/414899#M62240</guid>
      <dc:creator>sammypeiren</dc:creator>
      <dc:date>2015-11-17T12:17:01Z</dc:date>
    </item>
  </channel>
</rss>