<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 VPU encoder feature</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-encoder-feature/m-p/414616#M62162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; The VPU of the i.MX6 can decode two streams of 1080p@30 for MPEG4 / H.264.&lt;/P&gt;&lt;P&gt;&amp;nbsp; The VPU of the i.MX6 can encode single stream of 1080p@30 for MPEG4 / H.264.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; The VPU of the i.MX6 can decode four streams of 720p@30 for MPEG4 / H.264.&lt;/P&gt;&lt;P&gt;&amp;nbsp; The VPU of the i.MX6 can encode three streams of 720p@30 for MPEG4 / H.264.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We cannot guarantee 1920x1088@30fps plus D1@30fps H264 encoding.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jul 2015 02:55:55 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-07-16T02:55:55Z</dc:date>
    <item>
      <title>i.MX6 VPU encoder feature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-encoder-feature/m-p/414615#M62161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chip Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think typical surveillance IP camera today supports 1080p30+D1 of h264@BP encoding.&lt;BR /&gt;So I want to confirm i.MX6S VPU H264 encoder features.&lt;BR /&gt;Compared to the i.MX6SDL RM Rev1 and Rev2, VPU feature updated as following.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rev1: It can also perform H.264 BP/CBP, ... encoding up to @30fps. &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; VPU can support encode or decode multiple video clips with multiple standards simultaneously.&lt;/P&gt;&lt;P&gt;Rev2: The supported resolution is up to ... full-HD 1920x1088@30fps for encoding ... &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; VPU can support ...and also support multiple decoding and ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Q) Can i.MX6S VPU support multiple H264 encoding?&lt;BR /&gt;(Q) If yes, can i.MX6S VPU support 1920x1088@30fps plus D1@30fps H264 encoding?&lt;BR /&gt;(Q) Can i.MX6DLor6Q VPU support 1920x1088@30fps plus D1@30fps H264 encoding?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 11:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-encoder-feature/m-p/414615#M62161</guid>
      <dc:creator>torus1000</dc:creator>
      <dc:date>2015-07-15T11:00:08Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 VPU encoder feature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-encoder-feature/m-p/414616#M62162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; The VPU of the i.MX6 can decode two streams of 1080p@30 for MPEG4 / H.264.&lt;/P&gt;&lt;P&gt;&amp;nbsp; The VPU of the i.MX6 can encode single stream of 1080p@30 for MPEG4 / H.264.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; The VPU of the i.MX6 can decode four streams of 720p@30 for MPEG4 / H.264.&lt;/P&gt;&lt;P&gt;&amp;nbsp; The VPU of the i.MX6 can encode three streams of 720p@30 for MPEG4 / H.264.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We cannot guarantee 1920x1088@30fps plus D1@30fps H264 encoding.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2015 02:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-encoder-feature/m-p/414616#M62162</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-07-16T02:55:55Z</dc:date>
    </item>
  </channel>
</rss>