<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 SPI 3-Wire in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SPI-3-Wire/m-p/414558#M62149</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I didn't try this connection (SPI 4-wire to SPI 3-wire). So I cannot tell you the above design can work or not.&lt;/P&gt;&lt;P&gt;I tried to porting a LCD panel (SPI 3-wire). I just connect the MOSI to the LCD panel's SDA pin because I don't need to read the message from the panel to make it work.&lt;/P&gt;&lt;P&gt;I think another method is using GPIO pins as SPI. I remember there is GPIO-SPI in linux already. I think you may modify the code little bit so you may able to change GPIO read/write for the SPI read/write. Hope this information can help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 May 2015 09:34:44 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2015-05-11T09:34:44Z</dc:date>
    <item>
      <title>IMX6 SPI 3-Wire</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SPI-3-Wire/m-p/414557#M62148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Currently I am having an IMX6 board connected with LCD controller via SPI as shown below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31107i4FFF4AA1A66DB3DE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here SDO and SDI on Slave side are connected together via a resistor to the slave. Hence the SPI interface is 3- Wire.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read some posts saying that for SPI 3-Wire to work, we need to connect MOSI to MISO via resistor, which is not the case above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can some one please tell me whether the above design will work for SPI 3-Wire ?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 May 2015 07:45:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SPI-3-Wire/m-p/414557#M62148</guid>
      <dc:creator>jamesdeepu</dc:creator>
      <dc:date>2015-05-09T07:45:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 SPI 3-Wire</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-SPI-3-Wire/m-p/414558#M62149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I didn't try this connection (SPI 4-wire to SPI 3-wire). So I cannot tell you the above design can work or not.&lt;/P&gt;&lt;P&gt;I tried to porting a LCD panel (SPI 3-wire). I just connect the MOSI to the LCD panel's SDA pin because I don't need to read the message from the panel to make it work.&lt;/P&gt;&lt;P&gt;I think another method is using GPIO pins as SPI. I remember there is GPIO-SPI in linux already. I think you may modify the code little bit so you may able to change GPIO read/write for the SPI read/write. Hope this information can help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2015 09:34:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-SPI-3-Wire/m-p/414558#M62149</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2015-05-11T09:34:44Z</dc:date>
    </item>
  </channel>
</rss>