<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question, i.MX25 NAND</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414220#M62084</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Basically, the customer believes that the ECC feature does not need to be set to 'disable' in i.MX25 side.&lt;/P&gt;&lt;P&gt;They believes the conflict will not occur because the algorithm of ECC on BENAND differs from i.MX25.&lt;/P&gt;&lt;P&gt;And they believe the point is that i.MX25 must support the ‘collective programming’ which is needed for BENAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The customer’s understanding is as below.&lt;/P&gt;&lt;P&gt;Are those correct?&lt;/P&gt;&lt;P&gt;I think that there are differences from your opinion.&lt;/P&gt;&lt;P&gt;Could you give your comment on that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1)&lt;/P&gt;&lt;P&gt;i.MX25 NFC can support the programming method which is needed for the BENAND.&lt;/P&gt;&lt;P&gt;The BENAND must be programmed en bloc of 512+16Byte at a time, as mentioned in the attached file in the original posting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2)&lt;/P&gt;&lt;P&gt;The algorithms of handling ECC differ between the BENAND and i.MX25 NFC.&lt;/P&gt;&lt;P&gt;For the BENAND, ECC is calculated for every 512+16Byte and the ECC is written in the special area in the BENAND.&lt;/P&gt;&lt;P&gt;For i.MX25 NFC, ECC is calculated for every 512byte main area and the ECC is written into 16Byte spare area.&lt;/P&gt;&lt;P&gt;Then, the ECC algorithms of the BENAND and i.MX25 will run separately.&lt;/P&gt;&lt;P&gt;The conflict will not occur between the algorithms of BENAND and i.MX25 NFC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(3)&lt;/P&gt;&lt;P&gt;They believes that the BENAND can be used for i.MX25 boot.&lt;/P&gt;&lt;P&gt;One can use the following setting for the BENAND.&lt;/P&gt;&lt;P&gt;BMOD[1:0]=00&lt;/P&gt;&lt;P&gt;SLC_NAND/128Byte_spare_for_4kByte/page_size=2kByte&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(4)&lt;/P&gt;&lt;P&gt;The customer believes that BENAND can be used for boot device of i.MX25.&lt;/P&gt;&lt;P&gt;BTW, they are using Linux OS, and uboot, kernel and rootfs are written in the NAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Nov 2015 07:35:00 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-11-25T07:35:00Z</dc:date>
    <item>
      <title>Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414216#M62080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about NAND Flash which can be used for i.MX257.&lt;/P&gt;&lt;P&gt;My customer is thinking about the use of Toshiba/BENAND, TC58BVG0S3HTAI0, for their custom i.MX25 board.&lt;/P&gt;&lt;P&gt;Could you show me whether the NAND chip can be used for i.MX25?&lt;/P&gt;&lt;P&gt;Please find the attached file for datasheet. It has 2048 Page size + 64 Spare size.&lt;/P&gt;&lt;P&gt;If it can be used for i.MX25,&lt;/P&gt;&lt;P&gt;The NAND flash has Built-in ECC feature. Then, the customer thinks the ECC feature in i.MX25 side will not be needed.&lt;/P&gt;&lt;P&gt;Is it possible to disable ECC feature in i.MX25 side?&lt;/P&gt;&lt;P&gt;Please show me the way to disable ECC feature on i.MX25.&lt;/P&gt;&lt;P&gt;In addition, the BENAND has a restriction on writing data as the attached file.&lt;/P&gt;&lt;P&gt;I think NFC or MFGTOOLS has to support the programming sequence of the BENAND.&lt;/P&gt;&lt;P&gt;If any concerns, please let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Nov 2015 08:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414216#M62080</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-11-16T08:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414217#M62081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; I am afraid it is impossible to disable i.MX25 NFC ECC. &lt;BR /&gt; Some NAND parts have option to disable internal ECC via SET FEATURE command,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;bit internal i.MX25 boot ROM does not perform it. As result flashes with internal ECC&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;cannot be used for boot under i.MX25.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Nov 2015 07:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414217#M62081</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-11-17T07:01:34Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414218#M62082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your comment.&lt;/P&gt;&lt;P&gt;The customer believes it is not a problem that i.MX25 cannot disable ECC.&lt;/P&gt;&lt;P&gt;They believe that if the specification around the page size and spare size of BENAND meet i.MX25 specification then the BENAND can be used.&lt;/P&gt;&lt;P&gt;But their concern is the restriction on programming of the BENAND.&lt;/P&gt;&lt;P&gt;The BENAND has a restriction on its programming as I mentioned in the attached file in original posting.&lt;/P&gt;&lt;P&gt;Could you give your comment on that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 06:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414218#M62082</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-11-20T06:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414219#M62083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; At least one of ECC support must be disabled : of i.MX25 or BENAND, since&lt;/P&gt;&lt;P&gt;ECC algorithm and data / spare layout should be just the same for both &lt;/P&gt;&lt;P&gt;i.MX25 NFC and BENAND to avoid issues. I have some doubt if i.MX25 NFC &lt;BR /&gt;and BENAND meet each other regarding ECC algorithm and data / spare layout.&lt;BR /&gt; &lt;BR /&gt;If BENAND ECC can be disabled in software - this means we cannot use the nand &lt;BR /&gt;during boot, but can - just for storing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 06:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414219#M62083</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-11-24T06:15:35Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414220#M62084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Basically, the customer believes that the ECC feature does not need to be set to 'disable' in i.MX25 side.&lt;/P&gt;&lt;P&gt;They believes the conflict will not occur because the algorithm of ECC on BENAND differs from i.MX25.&lt;/P&gt;&lt;P&gt;And they believe the point is that i.MX25 must support the ‘collective programming’ which is needed for BENAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The customer’s understanding is as below.&lt;/P&gt;&lt;P&gt;Are those correct?&lt;/P&gt;&lt;P&gt;I think that there are differences from your opinion.&lt;/P&gt;&lt;P&gt;Could you give your comment on that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1)&lt;/P&gt;&lt;P&gt;i.MX25 NFC can support the programming method which is needed for the BENAND.&lt;/P&gt;&lt;P&gt;The BENAND must be programmed en bloc of 512+16Byte at a time, as mentioned in the attached file in the original posting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2)&lt;/P&gt;&lt;P&gt;The algorithms of handling ECC differ between the BENAND and i.MX25 NFC.&lt;/P&gt;&lt;P&gt;For the BENAND, ECC is calculated for every 512+16Byte and the ECC is written in the special area in the BENAND.&lt;/P&gt;&lt;P&gt;For i.MX25 NFC, ECC is calculated for every 512byte main area and the ECC is written into 16Byte spare area.&lt;/P&gt;&lt;P&gt;Then, the ECC algorithms of the BENAND and i.MX25 will run separately.&lt;/P&gt;&lt;P&gt;The conflict will not occur between the algorithms of BENAND and i.MX25 NFC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(3)&lt;/P&gt;&lt;P&gt;They believes that the BENAND can be used for i.MX25 boot.&lt;/P&gt;&lt;P&gt;One can use the following setting for the BENAND.&lt;/P&gt;&lt;P&gt;BMOD[1:0]=00&lt;/P&gt;&lt;P&gt;SLC_NAND/128Byte_spare_for_4kByte/page_size=2kByte&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(4)&lt;/P&gt;&lt;P&gt;The customer believes that BENAND can be used for boot device of i.MX25.&lt;/P&gt;&lt;P&gt;BTW, they are using Linux OS, and uboot, kernel and rootfs are written in the NAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Nov 2015 07:35:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414220#M62084</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-11-25T07:35:00Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414221#M62085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Really NAND layout for the BENAND and i.MX25 is not the same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt; BENAND : 512 bytes + 512 bytes + 512 bytes +512 bytes + spare bytes&lt;BR /&gt; + spare bytes + …&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;BR /&gt; i.MX25 : 512 bytes main + spare bytes + 512 bytes main + spare bytes +&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;512 bytes main +spare bytes + ...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;2.&lt;BR /&gt; The algorithms of handling ECC differ between the BENAND and i.MX25 NFC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;This definitely does not allow to use them simultaneously. Although ECC algorithms &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;can work separately, but results (sum and location) will not be the same and &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;any ECC modifications of BENAND will treated as error by the i.MX25 and vise versa.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;3.&lt;BR /&gt; The i.MX25 can boot the NAND only if ECC is correct, that is – written by the i.MX25&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;itself, without any modification by the internal NAND controller.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;4.&lt;BR /&gt; If the NAND is already working – this means, that really ECC algorithm and layout&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;for the i.MX25 and the NAND are the same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 07:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414221#M62085</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-12-03T07:37:46Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414222#M62086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for my late response.&lt;/P&gt;&lt;P&gt;But the customer is still thinking about the use of the BENAND with i.MX25.&lt;/P&gt;&lt;P&gt;The customer found the following description in i.MX25 reference manual.&lt;/P&gt;&lt;P&gt;“The ECC operation can be bypassed using ECC_EN bit in CONFIG1 register.”&lt;/P&gt;&lt;P&gt;The customer thinks i.MX25 NFC can access the BENAND as 512+512+512+512+64 without checking ECC, when the page-size is 2K bytes, by setting the ECC_EN bit.&lt;/P&gt;&lt;P&gt;Is it true?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks so much,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 04:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414222#M62086</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-12-22T04:06:32Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414223#M62087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; Yes, if&amp;nbsp; ECC_EN bit in CONFIG1 register is cleared, the ECC functionality of the i.MX25 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;is totally idle. The problem is how to disable it during boot. To get some register &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;settings during boot via DCD, requires at least to read boot NAND, assuming by default&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;ECC is enabled. That is, the first pages of NAND must have correct ECC.&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 06:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414223#M62087</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-12-22T06:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414224#M62088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your comment.&lt;/P&gt;&lt;P&gt;The customer expects that;&lt;/P&gt;&lt;P&gt;i.MX25 can access as the following NAND layout by setting (clear) the ECC_EN bit,&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt; BENAND : 512 bytes + 512 bytes + 512 bytes +512 bytes + spare bytes&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt; + spare bytes + &lt;SPAN lang="EN-US" style="font-family: 'Courier New';"&gt;…&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Courier New';"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Courier New';"&gt;even though, i.MX25 access NAND as below.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;&amp;gt;&amp;gt;&amp;gt; i.MX25 : 512 bytes main + spare bytes + 512 bytes main + spare bytes&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt; + 512 bytes main +spare bytes + ...&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that the difference on the NAND layout between BENAND and i.MX25 NFCis still the problem whether the ECC_EN setting is 1 or 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Dec 2015 11:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414224#M62088</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-12-24T11:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX25 NAND</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414225#M62089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Alas, i.MX25 cannot use the following NAND layout by setting (clear) the ECC_EN bit,&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;512 bytes + 512 bytes + 512 bytes +512 bytes + spare bytes + spare bytes + &lt;SPAN lang="EN-US" style="font-weight: inherit; font-style: inherit; font-family: 'Courier New';"&gt;…&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The i.MX25 NFC is the same for ECC enabled or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 08:31:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX25-NAND/m-p/414225#M62089</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-01-13T08:31:02Z</dc:date>
    </item>
  </channel>
</rss>