<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RTC in the iMX537 cpu</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173961#M6206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;in which file we need to change this??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Sep 2012 07:40:56 GMT</pubDate>
    <dc:creator>Gokul</dc:creator>
    <dc:date>2012-09-10T07:40:56Z</dc:date>
    <item>
      <title>RTC in the iMX537 cpu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173957#M6202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;we developed a custom board with the iMX537 and the PMIC MC34708 chip.&lt;/P&gt;&lt;P&gt;On the PMIC, there is a coin cell connected (3V CR2032) on the LICELL pin.&lt;/P&gt;&lt;P&gt;If we program the RTC on the CPU, the RTC runs perfect until we cut the power, afterwards, all the RTC registers are reset.&lt;/P&gt;&lt;P&gt;We have tried the same on a (changed) QSBoard and have the same behavior.&lt;/P&gt;&lt;P&gt;While the power is cut, the voltage VSRTS drops from 1.3V to 1.23V and the 32Khz clock keeps running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anbody who has already successfull used the iMX537 RTC function, so yes can you give me any sugestion where to look for ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Johan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jul 2012 07:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173957#M6202</guid>
      <dc:creator>jomeke</dc:creator>
      <dc:date>2012-07-11T07:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: RTC in the iMX537 cpu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173958#M6203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Johan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use the iMX535 and have a similar (probably the same)&amp;nbsp;issue - I assume we are dealing with the same problem.&lt;/P&gt;&lt;P&gt;First, look at the Errata sheet for your processor. For the iMX535, errata #23 identifies this&amp;nbsp;exact problem. The workaround is to connect an additional circuit to VDDLP pin on the PMIC (shown in errata sheet), however, when we have done that we experienced a rapid battery drain - we are currently investigating how to solve this problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2012 22:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173958#M6203</guid>
      <dc:creator>marek1z</dc:creator>
      <dc:date>2012-09-04T22:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: RTC in the iMX537 cpu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173959#M6204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How did you program your RTC and which RTC did you program?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you program the RTC on the PMIC or the SRTC on the i.MX537?&lt;/P&gt;&lt;P&gt;If you are using Linux, RTC0 will be the processor SRTC and RTC1 will be the PMIC RTC.&amp;nbsp; You will want to use the PMIC RTC ( RTC1 ) for your coin cell backed up RTC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2012 17:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173959#M6204</guid>
      <dc:creator>JohnGoodman</dc:creator>
      <dc:date>2012-09-05T17:38:13Z</dc:date>
    </item>
    <item>
      <title>Re: RTC in the iMX537 cpu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173960#M6205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is the answer that we received from Freescale :&lt;/P&gt;&lt;P&gt;In reply to your Service Request SR 1-894779544:&lt;BR /&gt;&lt;BR /&gt;OK, Got it. Some customers also met the same problem. I just now adjusted power up sequence. Do it like this :&lt;BR /&gt;VDD_DIG_PLL(1.3v) supplies for VDDA and 1V3_VGEN1 supplies for VDDAL, SRTC can be kept after cold reset. So please retry it !&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2012 06:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173960#M6205</guid>
      <dc:creator>jomeke</dc:creator>
      <dc:date>2012-09-06T06:36:00Z</dc:date>
    </item>
    <item>
      <title>Re: RTC in the iMX537 cpu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173961#M6206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;in which file we need to change this??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2012 07:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173961#M6206</guid>
      <dc:creator>Gokul</dc:creator>
      <dc:date>2012-09-10T07:40:56Z</dc:date>
    </item>
    <item>
      <title>Re: RTC in the iMX537 cpu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173962#M6207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; Please refer to ENGcm12374 (SRTC loses data while powering up/down)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;from the Errata.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/errata/IMX53CE.pdf" rel="nofollow"&gt;http://cache.freescale.com/files/32bit/doc/errata/IMX53CE.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 02:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RTC-in-the-iMX537-cpu/m-p/173962#M6207</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-06T02:28:07Z</dc:date>
    </item>
  </channel>
</rss>