<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Initializing UART1 after raw boot from SD-Card - iMX.6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Initializing-UART1-after-raw-boot-from-SD-Card-iMX-6/m-p/413805#M62003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is recommended to check that uart clocks are enabled in CCM_CCGRn registers, then&lt;/P&gt;&lt;P&gt;one can try to run OS-less UART1 test code with SDK (one can run it with jtag),&lt;/P&gt;&lt;P&gt;recommended to check signals with oscilloscope&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt;&amp;nbsp; : Bare-metal SDK for the i.MX 6&lt;/P&gt;&lt;P&gt;then compare SDK register settings with uboot/linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jun 2015 11:56:27 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-06-19T11:56:27Z</dc:date>
    <item>
      <title>Initializing UART1 after raw boot from SD-Card - iMX.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Initializing-UART1-after-raw-boot-from-SD-Card-iMX-6/m-p/413804#M62002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on low-level boot code. The first thing I need to do is get some debug out of UART1. So far I can't get a signal out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tx line is CSI0_DATA10, Rx line is CSI0_DATA11... although at this point I am not interested in input. I am sure I have the right pins, as I ran a test with it switched to GPIO mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For both lines MUX is set to Alt3, and PAD_CTL to 0x0001b0b0, the UART1_RX daisy chain is set to 0 (although I tried all four values).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am monitoring the TRDY in USR1 and writing bytes to UTXD when its set. By toggling an LED after an appropriate number of writes, I can tell that the UART module is working fine and set to the right baud rate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other than the MUX, CTL and daisy chain regs, is there anything else that controls/inhibits signals from the UART pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2015 03:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Initializing-UART1-after-raw-boot-from-SD-Card-iMX-6/m-p/413804#M62002</guid>
      <dc:creator>adrianthewlis</dc:creator>
      <dc:date>2015-06-19T03:49:31Z</dc:date>
    </item>
    <item>
      <title>Re: Initializing UART1 after raw boot from SD-Card - iMX.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Initializing-UART1-after-raw-boot-from-SD-Card-iMX-6/m-p/413805#M62003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is recommended to check that uart clocks are enabled in CCM_CCGRn registers, then&lt;/P&gt;&lt;P&gt;one can try to run OS-less UART1 test code with SDK (one can run it with jtag),&lt;/P&gt;&lt;P&gt;recommended to check signals with oscilloscope&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt;&amp;nbsp; : Bare-metal SDK for the i.MX 6&lt;/P&gt;&lt;P&gt;then compare SDK register settings with uboot/linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2015 11:56:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Initializing-UART1-after-raw-boot-from-SD-Card-iMX-6/m-p/413805#M62003</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-19T11:56:27Z</dc:date>
    </item>
  </channel>
</rss>