<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GPU to CPU copy taking long time in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPU-to-CPU-copy-taking-long-time/m-p/413429#M61927</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abhilash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of such patch but one can try solutions below for improving&lt;/P&gt;&lt;P&gt;memcpy copy time&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="340705" data-objecttype="1" href="https://community.freescale.com/thread/340705"&gt;https://community.freescale.com/thread/340705&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://allontutorials.com/benchmarking-the-gpu-bandwidth-capability-based-on-opencl-memory-copy-operation/" rel="nofollow"&gt;http://allontutorials.com/benchmarking-the-gpu-bandwidth-capability-based-on-opencl-memory-copy-operation/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Sep 2015 11:38:07 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-09-28T11:38:07Z</dc:date>
    <item>
      <title>GPU to CPU copy taking long time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-to-CPU-copy-taking-long-time/m-p/413428#M61926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using IMX6Q and has no display. I'm doing a capture of Y16 format with 1040*768 pixels. I want to use the GPU for the processing. As a start point I configured the shaders in such a way to just pass the capture through GPU without any change in pixels. I have used glTexImage2D with the v4l2 buffer as input. The display I have configured is the framebuffer and I'm able to get the frames to framebuffer. I did a mmap to read the framebuffer to the application for streaming. I could find that the memcpy was taking 12ms for 1040*768*2 bytes. Is there any means to improve it? I'm using yocto with Linux 3.10.17.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Sep 2015 09:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-to-CPU-copy-taking-long-time/m-p/413428#M61926</guid>
      <dc:creator>abhilashabraham</dc:creator>
      <dc:date>2015-09-28T09:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: GPU to CPU copy taking long time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPU-to-CPU-copy-taking-long-time/m-p/413429#M61927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abhilash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of such patch but one can try solutions below for improving&lt;/P&gt;&lt;P&gt;memcpy copy time&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="340705" data-objecttype="1" href="https://community.freescale.com/thread/340705"&gt;https://community.freescale.com/thread/340705&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://allontutorials.com/benchmarking-the-gpu-bandwidth-capability-based-on-opencl-memory-copy-operation/" rel="nofollow"&gt;http://allontutorials.com/benchmarking-the-gpu-bandwidth-capability-based-on-opencl-memory-copy-operation/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Sep 2015 11:38:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPU-to-CPU-copy-taking-long-time/m-p/413429#M61927</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-28T11:38:07Z</dc:date>
    </item>
  </channel>
</rss>