<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Chromium-Browser in Yocto with Touch-Keyboard in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413175#M61889</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We'd like to integrate the Chromium-Browser in our Yocto-OS-Images for our i.MX6-based devices (using the "meta-browser" Yocto-layer). This works already quite well (with Chromium versions 40, 41, 42, and 43), but we have trouble getting a virtual touch-keyboard working to allow text input in web-pages. All our devices are equipped with resistive or capacitive touchscreens and none of our customers is using our devices with real hardware keyboards. Therefore we need to provide virtual soft-keyboards on the display, which can be be used via the touchscreen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While the more or less full desktop Yocto-configurations (with the "sato" or "xfce" desktops) do provide working soft-keyboards, it seems that these must always be shown and hidden manually by the user using the desktop-panel/-dock. These keyboards don't open/close automatically when you select a text-input field in the Chromium browser, and when you start Chromium in "kiosk"-mode (i.e. without GUI-decoration, URL-address-line, etc), as most of our customers demand, these soft-keyboards don't seem to work at all. You can't even open them, because the desktop-panel is not shown on the display (on purpose), when Chromium is running in kiosk-mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While Chromium itself seems to include code for its own private soft-keyboard in the Chromium source-tree, and provides command-line options like "--enable-virtual-keyboard", this presumed Chromium-internal soft-keyboard doesn't seem to work, either. Adding debugging messages to the corresponding Chromium source-code shows, that it doesn't even seem to try calling the soft-keyboard functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using Chromium-Extensions we have also been only partially successful: &lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Using the "Google Input Tool" extension, which several online forums recommend, doesn't seem to work, at all: Most of the time we're unable this keyboard at all, an even when it does pop-up occasionally, button presses don't get sent to the selected text-input fields&lt;/LI&gt;&lt;LI&gt;Using the "Virtual Keyboard" extension from xontab.com found in the Chromium Web-Store works somewhat for most web-forms, but it fails completely e.g. for the search-form on &lt;A href="https://community.nxp.com/www.google.com" target="test_blank"&gt;www.google.com&lt;/A&gt; (opens briefly but closes immediately again before you're able to type even a single letter) and on forms, where it works, it often doesn't scroll the web-site properly when it opens, so that you don't see the text-input field you're typing into.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody have an idea, how to enable the Chromium-internal soft-keyboard or how to integrate one of the desktop virtual keyboards (like "matchbox-keyboard" or "xkb") in such a way into the system, that they pop-up automatically when selecting a text-input field in the Chromium browser? Or does anybody know better Chromium soft-keyboard extensions that work on all web-forms automatically?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Marc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 May 2015 09:24:03 GMT</pubDate>
    <dc:creator>MOW</dc:creator>
    <dc:date>2015-05-08T09:24:03Z</dc:date>
    <item>
      <title>Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413175#M61889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We'd like to integrate the Chromium-Browser in our Yocto-OS-Images for our i.MX6-based devices (using the "meta-browser" Yocto-layer). This works already quite well (with Chromium versions 40, 41, 42, and 43), but we have trouble getting a virtual touch-keyboard working to allow text input in web-pages. All our devices are equipped with resistive or capacitive touchscreens and none of our customers is using our devices with real hardware keyboards. Therefore we need to provide virtual soft-keyboards on the display, which can be be used via the touchscreen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While the more or less full desktop Yocto-configurations (with the "sato" or "xfce" desktops) do provide working soft-keyboards, it seems that these must always be shown and hidden manually by the user using the desktop-panel/-dock. These keyboards don't open/close automatically when you select a text-input field in the Chromium browser, and when you start Chromium in "kiosk"-mode (i.e. without GUI-decoration, URL-address-line, etc), as most of our customers demand, these soft-keyboards don't seem to work at all. You can't even open them, because the desktop-panel is not shown on the display (on purpose), when Chromium is running in kiosk-mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While Chromium itself seems to include code for its own private soft-keyboard in the Chromium source-tree, and provides command-line options like "--enable-virtual-keyboard", this presumed Chromium-internal soft-keyboard doesn't seem to work, either. Adding debugging messages to the corresponding Chromium source-code shows, that it doesn't even seem to try calling the soft-keyboard functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using Chromium-Extensions we have also been only partially successful: &lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Using the "Google Input Tool" extension, which several online forums recommend, doesn't seem to work, at all: Most of the time we're unable this keyboard at all, an even when it does pop-up occasionally, button presses don't get sent to the selected text-input fields&lt;/LI&gt;&lt;LI&gt;Using the "Virtual Keyboard" extension from xontab.com found in the Chromium Web-Store works somewhat for most web-forms, but it fails completely e.g. for the search-form on &lt;A href="https://community.nxp.com/www.google.com" target="test_blank"&gt;www.google.com&lt;/A&gt; (opens briefly but closes immediately again before you're able to type even a single letter) and on forms, where it works, it often doesn't scroll the web-site properly when it opens, so that you don't see the text-input field you're typing into.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody have an idea, how to enable the Chromium-internal soft-keyboard or how to integrate one of the desktop virtual keyboards (like "matchbox-keyboard" or "xkb") in such a way into the system, that they pop-up automatically when selecting a text-input field in the Chromium browser? Or does anybody know better Chromium soft-keyboard extensions that work on all web-forms automatically?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Marc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 09:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413175#M61889</guid>
      <dc:creator>MOW</dc:creator>
      <dc:date>2015-05-08T09:24:03Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413176#M61890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marc,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are discussing internally about your issue, as soon as we have a response, we will back to you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 15:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413176#M61890</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2015-05-20T15:03:29Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413177#M61891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marc-Oliver,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At O.S. Systems we've been supporting some customers using Chromium and as well our i.MX6 enabled QtWebEngine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your description it is clear that you would benefit of using the QtWebEngine as you could run it in EGLFS and avoid all the boilerplate of X environment. This could also rely on a QML virtual keyboard and do a much more polished product.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want assistance with Chromium and/or QtWebEngine please contact me privately and we can move on, on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 17:32:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413177#M61891</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2015-05-20T17:32:14Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413178#M61892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Otavio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you also have a proper soft-keyboard solution for Chromium, which also works with current stable Chromium releases? Our customers prefer Chromium to the QtWebEngine due to far better HTML5-support, significantly higher rendering performance and easier web-app development, as customers can test and debug their web-applications easily with the regular Chrome-Desktop-Browser on their PCs already.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2015 09:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413178#M61892</guid>
      <dc:creator>MOW</dc:creator>
      <dc:date>2015-06-11T09:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413179#M61893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We did this integration for one project, yes. However we have been way more successful using QtWebEngine than plan Chromium in many projects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want, we can have a short talk to discuss each approach and its pros and cons. If necessary we can explore the possible solutions but we need to better understand the use-cases involved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2015 11:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413179#M61893</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2015-06-11T11:36:49Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413180#M61894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Otavio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also currently trying&amp;nbsp; to get a soft-keyboard for chromium working, is this something you are willing to share?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 07:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413180#M61894</guid>
      <dc:creator>davidlockyer</dc:creator>
      <dc:date>2015-06-18T07:59:46Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413181#M61895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We did this for some projects of customers. We wrote a virtual keyboard for some of them (for those running on top of X11) and did apps using WebEngine which had virtual keyboards as part of them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is all customer-related work, nothing of this is opensource from our side. Sorry.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2015 17:28:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413181#M61895</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2015-07-03T17:28:20Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413182#M61896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having the same problem. Did you find a solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Nik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 08:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413182#M61896</guid>
      <dc:creator>nikhersche</dc:creator>
      <dc:date>2016-01-15T08:55:56Z</dc:date>
    </item>
    <item>
      <title>Re: Chromium-Browser in Yocto with Touch-Keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413183#M61897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not really. But our customers seem to be happy with the "Virtual Keyboard" from xontab found in the Chromium store, so far.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only information we figured out regarding the "official" soft-keyboard of the Chromium browser is, that it seems to be intended to be used only together with the full Chromium-OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards Marc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Feb 2016 08:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Chromium-Browser-in-Yocto-with-Touch-Keyboard/m-p/413183#M61897</guid>
      <dc:creator>MOW</dc:creator>
      <dc:date>2016-02-11T08:53:39Z</dc:date>
    </item>
  </channel>
</rss>