<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx6  system wake up</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-system-wake-up/m-p/413130#M61871</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Robert&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think one can look at unit tests mxc_rtc test (wake-up after some time)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.53-1.1.0/" title="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.53-1.1.0/"&gt;Index of /buildsources/i/imx-test/imx-test-3.10.53-1.1.0&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Jun 2015 00:25:02 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-06-01T00:25:02Z</dc:date>
    <item>
      <title>imx6  system wake up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-system-wake-up/m-p/413129#M61870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking for information on how to run imx6solo light in low power mode and deep sleep for 1/2 my processing time.&lt;/P&gt;&lt;P&gt;I can command my custom board into deep sleep mode (refer to AN4580) but have not set-up a wake up time.&amp;nbsp; I am looking for instructions on how to set up the wake time after I command the power state to "mem"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also looking to run very low power, with 1 G of LP DDR2&amp;nbsp; my board is pulling about 33 mA of the 56 mA total load.&amp;nbsp; Any suggestions on reducing the memory power consumption?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2015 21:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-system-wake-up/m-p/413129#M61870</guid>
      <dc:creator>RobertCorrellus</dc:creator>
      <dc:date>2015-05-29T21:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx6  system wake up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-system-wake-up/m-p/413130#M61871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Robert&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think one can look at unit tests mxc_rtc test (wake-up after some time)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.53-1.1.0/" title="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.53-1.1.0/"&gt;Index of /buildsources/i/imx-test/imx-test-3.10.53-1.1.0&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2015 00:25:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-system-wake-up/m-p/413130#M61871</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-01T00:25:02Z</dc:date>
    </item>
  </channel>
</rss>