<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックEnter Recovery Mode Through JTAG</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enter-Recovery-Mode-Through-JTAG/m-p/412993#M61844</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to enter recovery mode on i.MX6 Solo and DualLite through some JTAG commands. I'm looking for the easiest way possible, as we plan to use a bit-bang JTAG approach without&amp;nbsp; any predefined configuration files, etc like would be available on e.g. Lauterbach. I'm thinking about a simple IR and DR combination to modify the GPR9 and 10 register. Or a simple way of loading a small assembler code into internal ram and execute this. Any solution is OK as long as it can be done through JTAG only.&lt;/P&gt;&lt;P&gt;We would like to enter recovery mode on a device where the HW recovery mode (BOOT_MODE0) pin isn't available.&lt;/P&gt;&lt;P&gt;We just started looking at this, so any input or suggestion might be helpful.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Roman&lt;/P&gt;&lt;P&gt;Toradex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 May 2015 07:33:14 GMT</pubDate>
    <dc:creator>romanschnarwile</dc:creator>
    <dc:date>2015-05-08T07:33:14Z</dc:date>
    <item>
      <title>Enter Recovery Mode Through JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enter-Recovery-Mode-Through-JTAG/m-p/412993#M61844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to enter recovery mode on i.MX6 Solo and DualLite through some JTAG commands. I'm looking for the easiest way possible, as we plan to use a bit-bang JTAG approach without&amp;nbsp; any predefined configuration files, etc like would be available on e.g. Lauterbach. I'm thinking about a simple IR and DR combination to modify the GPR9 and 10 register. Or a simple way of loading a small assembler code into internal ram and execute this. Any solution is OK as long as it can be done through JTAG only.&lt;/P&gt;&lt;P&gt;We would like to enter recovery mode on a device where the HW recovery mode (BOOT_MODE0) pin isn't available.&lt;/P&gt;&lt;P&gt;We just started looking at this, so any input or suggestion might be helpful.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Roman&lt;/P&gt;&lt;P&gt;Toradex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 07:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enter-Recovery-Mode-Through-JTAG/m-p/412993#M61844</guid>
      <dc:creator>romanschnarwile</dc:creator>
      <dc:date>2015-05-08T07:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: Enter Recovery Mode Through JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enter-Recovery-Mode-Through-JTAG/m-p/412994#M61845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roman&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;suggest to look at link&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/409018"&gt;Use JTAG to force entry into Serial Downloader mode&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 10:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enter-Recovery-Mode-Through-JTAG/m-p/412994#M61845</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-05-08T10:36:33Z</dc:date>
    </item>
    <item>
      <title>Re: Enter Recovery Mode Through JTAG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enter-Recovery-Mode-Through-JTAG/m-p/412995#M61846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks. I didn't find that post. Looks promising, we'll l give it a try. I try to update this post here with our findings, but give me some time.&lt;/P&gt;&lt;P&gt;Have a nice weekend&lt;/P&gt;&lt;P&gt;Roman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 16:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enter-Recovery-Mode-Through-JTAG/m-p/412995#M61846</guid>
      <dc:creator>romanschnarwile</dc:creator>
      <dc:date>2015-05-08T16:29:36Z</dc:date>
    </item>
  </channel>
</rss>