<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is there i.MX6 Platform SDK for Linux? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-i-MX6-Platform-SDK-for-Linux/m-p/411279#M61641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&amp;nbsp; i.MX 6 Series Platform SDK&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&amp;nbsp; is ”bare-metal SDK for the i.MX 6 series, including reusable drivers &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;and tests for many peripherals, and much example code. Also includes register definition headers files, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;and register definitions for debuggers”.&lt;BR /&gt; As for Linux, please use examples in "unit_tests" directory.&lt;BR /&gt; &lt;/SPAN&gt; &lt;/P&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; The unit tests comes with the BSP (LTIB or Yocto). The binaries are located at &lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;rootfs/unit_tests and the source code you can get with the LTIB command:&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;$ ./ltib -p imx-test -m prep&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;the source will be located at &amp;lt;ltib folder&amp;gt;/rpm/BUILD/imx-test-&amp;lt;version&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Under Yocto there is imx-test recipe.&lt;BR /&gt; &lt;BR /&gt;&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;$ bitbake imx-test&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 May 2015 02:40:07 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-05-08T02:40:07Z</dc:date>
    <item>
      <title>Is there i.MX6 Platform SDK for Linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-i-MX6-Platform-SDK-for-Linux/m-p/411278#M61640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i.MX6 Platform SDK has very useful functions for developing, but it can not run under Linux.&lt;/P&gt;&lt;P&gt;Is it possible to migrate i.MX6 Platform SDK into Linux OS?&lt;/P&gt;&lt;P&gt;Or if there were similar library in Linux BSP, tell me the way to use them please.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 01:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-i-MX6-Platform-SDK-for-Linux/m-p/411278#M61640</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-05-08T01:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: Is there i.MX6 Platform SDK for Linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-i-MX6-Platform-SDK-for-Linux/m-p/411279#M61641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&amp;nbsp; i.MX 6 Series Platform SDK&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&amp;nbsp; is ”bare-metal SDK for the i.MX 6 series, including reusable drivers &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;and tests for many peripherals, and much example code. Also includes register definition headers files, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;and register definitions for debuggers”.&lt;BR /&gt; As for Linux, please use examples in "unit_tests" directory.&lt;BR /&gt; &lt;/SPAN&gt; &lt;/P&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; The unit tests comes with the BSP (LTIB or Yocto). The binaries are located at &lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;rootfs/unit_tests and the source code you can get with the LTIB command:&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;$ ./ltib -p imx-test -m prep&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;the source will be located at &amp;lt;ltib folder&amp;gt;/rpm/BUILD/imx-test-&amp;lt;version&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding: 0 0 24.0pt 0;"&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Under Yocto there is imx-test recipe.&lt;BR /&gt; &lt;BR /&gt;&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;$ bitbake imx-test&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 02:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-i-MX6-Platform-SDK-for-Linux/m-p/411279#M61641</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-05-08T02:40:07Z</dc:date>
    </item>
    <item>
      <title>Re: Is there i.MX6 Platform SDK for Linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-i-MX6-Platform-SDK-for-Linux/m-p/411280#M61642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please give the link to download platform SDK. I am working on IMX6UL-EVK and I want to port on bare metal. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;P&gt;Phani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2015 08:14:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-i-MX6-Platform-SDK-for-Linux/m-p/411280#M61642</guid>
      <dc:creator>phanikumar</dc:creator>
      <dc:date>2015-12-04T08:14:21Z</dc:date>
    </item>
  </channel>
</rss>