<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGstreamer questions</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-questions/m-p/410513#M61476</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using an IMX6Q 3.10.17.0 BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can freescale's Gstreamer 1.0 be ported to the 3.10.17 Kernel BSP?&lt;/P&gt;&lt;P&gt;My Gstreamer 0.10 doesn't have a videorate plugin. Is my base install broken?&lt;/P&gt;&lt;P&gt;Some of the element properties from tvsrc (ex. fps-n, do-timestamp do not work. Is my base install broken?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 May 2015 15:36:35 GMT</pubDate>
    <dc:creator>nmak</dc:creator>
    <dc:date>2015-05-07T15:36:35Z</dc:date>
    <item>
      <title>Gstreamer questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-questions/m-p/410513#M61476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using an IMX6Q 3.10.17.0 BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can freescale's Gstreamer 1.0 be ported to the 3.10.17 Kernel BSP?&lt;/P&gt;&lt;P&gt;My Gstreamer 0.10 doesn't have a videorate plugin. Is my base install broken?&lt;/P&gt;&lt;P&gt;Some of the element properties from tvsrc (ex. fps-n, do-timestamp do not work. Is my base install broken?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2015 15:36:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-questions/m-p/410513#M61476</guid>
      <dc:creator>nmak</dc:creator>
      <dc:date>2015-05-07T15:36:35Z</dc:date>
    </item>
    <item>
      <title>Re: Gstreamer questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-questions/m-p/410514#M61477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Nathan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;recommended to use latest BSP, it supports Gstreamer 1.0:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.14.28_1.0.0_iMX6QDLS_BUNDLE&lt;/A&gt; &lt;IMG alt="" class="jive-image" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; :&lt;/P&gt;&lt;P&gt;FSL BSP kernel 3.10.17 does not support Gstreamer 1.0,&lt;/P&gt;&lt;P&gt;one can refer to attached file, regarding porting suggest to look at&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/352482"&gt;Problems building i.MX6 image for LinuxFB with Dizzy BSP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 01:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-questions/m-p/410514#M61477</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-05-08T01:45:27Z</dc:date>
    </item>
    <item>
      <title>Re: Gstreamer questions</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-questions/m-p/410515#M61478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wish I could update the BST. Unfortunately we're well into development and running the update treadmill isn't appealing to us. Can you speak to any of my questions directly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 15:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-questions/m-p/410515#M61478</guid>
      <dc:creator>nmak</dc:creator>
      <dc:date>2015-05-08T15:06:15Z</dc:date>
    </item>
  </channel>
</rss>